Data Converters

Cross Reference

Application Notes

Training

Tools & Software

Block Diagrams

WEBENCH® Design Center

Wireless Infrastructure: Heterodyne RX/TX

Wireless Infrastructure: Heterodyne RX/TX

In the single-IF Heterodyne configurations, a digital up converter (DUC)/down converter (DDC) replaces the IF analog modulator/demodulator, which means no LO/carrier self-mixing at IF to obtain perfect gain/phase matching. Carrier/channel selection can be implemented in the digital domain (DUC/DDC). The single channel ADC/DAC does not receive/transmit a low frequency baseband signal, but an intermediate frequency (IF). The IF is defined by the frequency of the digital sine and cosine generator, which is a numerically controlled oscillator (NCO). The IF signal is up/down converted to/from RF through one analog mixing stage, reducing the RF BOM. The IF frequency is usually in the 70 MHz to 200 MHz range.

Benefits
  • No LO/carrier self-mixing at IF, perfect gain/phase matching, no offset.
  • High IF relaxes RF front-end image rejection filter requirement.
  • Reduces RF BOM (Bill of Materials).
  • Tradeoffs
  • High IF requires a wideband data converter, but ADC/DAC performance at such a high IF range limits the performance of such an architecture.
  • Carrier/channel selection can be implemented in the digital domain (DUC/DDC) but requires a high speed ADC/DAC.