com.ti.component.model.PageTitleValue@63290e1e

General Questions

  1. What are TINA and TINA-TI?
  2. What are the main differences between TINA-TI versions 7 and 9?
  3. Can I continue using TINA-TI version 7?
  4. Where do I get TINA-TI version 9?
  5. Where do I get the full version of TINA version 9 or upgrade TINA-TI version 9 to the full version of TINA?
  6. What are the minimum system requirements to run TINA-TI version 9?
  7. Where do I get TINA-TI help?
  8. How do I check for tool updates?

Simulation

  1. Where do I find TI device models and application circuits?
  2. Can TINA-TI run a circuit from another simulator?
  3. Can TINA-TI export a circuit to another simulator?
  4. How do I perform parametric analysis?
  5. How can I control the simulation accuracy and speed?

Waveform Display

  1. Can I probe a node voltage if I did not use a voltage meter prior to running the simulation?
  2. How do I change the simulation progress message mode?
  3. Does TINA-TI have a waveform measurement tool?
  4. How do I calculate a loop gain?
  5. How do I scale waveform in the display window?

Model and Circuit Development

  1. How do I edit a TINA device model symbol?
  2. Can I create a TINA library from TINA-TI?

What are TINA and TINA-TI?
TINA is a Spice-based circuit simulator running in the Microsoft Windows Operating system. It can do circuit DC, AC, Transient, Fourier, noise analysis, etc. TINA can be purchased through the vendor's (DesignSoft) web page located at www.tina.com.

TINA-TI is a simple version of TINA with full functionality in circuit simulation, but less circuit development utilities in the package. Also, TINA-TI contains more TI device models and TI part information. TI distributes TINA-TI free worldwide through www.ti.com/analogelab.

TINA-TI and TINA Design Suite Version Comparison

Program Feature TINA TINA-TI
Schematic entry and edit Yes Yes
Undo/Redo Yes Yes
Automatic/Manual wire routing and drag support Yes Yes
Instruments as standard schematic symbols Yes Yes
Sub-circuits Yes Yes
BOM Yes Yes
Bus Yes Yes
Integrated Net list Editor Yes Yes
Excitation Editor for arbitrary waveforms Yes Yes
Schematic Symbol Editor Yes Yes
Component Toolbar Editor Yes No
PCB export to major packages Yes No
Hierarchical and Team Design with version control Yes No
Parameter Extractor/Model Maker Yes No
PCB Design Yes No
Analyses
Max. number of external nodes and nodes in macros No limit No limit
DC, AC, Transient, Digital, Mixed mode simulation Yes Yes
Number of components and models 20,000 837 TI IC models and 236 National models plus other supporting devices
Group Delay Yes Yes
Parameter Sweeping Yes Yes
Analysis directly from Net list Yes Yes
Steady State Solver (SMPS analysis) Yes No
RF models given by S-parameters Yes No
Network Analysis Yes No
RF, Digital, VHDL, MCU Simulation Yes No
VHDL external debugger Yes No
Interactive Mode Yes No
Circuit changes while a simulation is running Yes No
Symbolic Analysis (Closed formulas) Yes No
Fourier Analysis (harmonics) Yes Yes
Fourier Analysis (spectrum) Yes No
Monte Carlo, Worst Case Yes Separate MC from Noise
Stress (Smoke) Analysis Yes No
Number of optimization targets & parameters No limit No
Number of parameters in parameter stepping No limit 1
Output Capabilities
Scaled Diagrams Yes Yes
Multiple Axes Yes Yes
Drawing tools to enhance diagrams Yes Yes
Post processing tools Yes Yes
Smith, Nyquist, Pole-Zero Diagram Yes No
Built-in DTP tools Yes No
MathCAD and Excel export Yes No
Virtual Instruments
XY Recorder, Oscilloscope, Function Generator, Multimeter, Signal Analyzer/Bode Plotter Yes Yes
Network, Spectrum, and Logic Analyzers Yes No
Digital Signal Generator Yes No
Real-time Test and Measurement Yes No
Educational Features Yes No
Back to top


What are the main differences between TINA-TI versions 7 and 9?
TINA-TI version 9 is a major upgrade of version 7. The main upgrades are in the following areas:

Back to top

Can I continue using TINA-TI version 7?
Version 7 will continue to be supported on a limited basis for a short period of time. Users are encouraged to download the latest version of TINA-TI to get all the benefits of version 9.

Circuits in TINA-TI version 7 will work on version 9. But, when a circuit is saved in version 9, it cannot be opened in version 7, unless the option to save as TINA v7 Schematic is selected in the File Save dialog box, as shown below.

Back to top

Where do I get TINA-TI version 9?
TINA-TI version 9 is distributed by TI. You can download it free from the TI website located at www.ti.com/analogelab.

Back to top

Where do I get the full version of TINA version 9 or upgrade TINA-TI version 9 to the full version of TINA?
The full version of TINA can be purchased from DesignSoft on the website located at www.tina.com. Users who currently have TINA-TI version 9 installed will receive a discount on the purchase of the full version.

NOTE: Please load the program within 7 days of purchase to avoid an expired download link.

Back to top

What are the minimum system requirements to run TINA-TI version 9?
The minimum hardware and software requirements for running TINA-TI version 9 are:

Back to top

Where do I get TINA-TI help?
There is basic help information in the tool that is accessible through the "Help" menu.

For help with TINA-TI related questions, please go to the vendor's website located at www.tina.com, or their support forums at DesignSoft Forum.

For TI device model related questions, post your question to TI E2E Community Simulation and Models Forum.

Back to top

How do I check for tool updates?
In order to check for updates, you must have TINA-TI version 9 or later.

From the menu:

  1. Click "Help"
  2. Select the option to "Check for Updates"
  3. If there are updates available, a screen will appear with the message: "New components detected". Click the "Update" button when the window appears on the screen.

The download site will appear. Follow the instructions to complete the update.

Back to top

Where do I find TI device models and application circuits?
TI device models and application circuits distributed with TINA-TI. From the installation directory, TI device circuits can be found in directory (tool installation directory)\examples\. Circuits in the directory are classified by applications. For example, directory\examples\SMPS\ contains TI switchmode power supply application circuits. Directory\examples\TI test circuits\ contains all TI linear device model test circuits.

TI device models are in the "Spice Macros" tab of the upper part of the main window (device bar). See video on how to insert a device model in a circuit. (NOTE: Video viewer needed to view example.)

Back to top

Can TINA-TI run a circuit from another simulator?
Yes, TINA-TI can import a circuit from another Spice simulator, but only in the form of a Spice netlist circuit. To run a Spice netlist circuit, open TINA-TI netlister from TINA's menu. Select "Tools", then "Netlist Editor". Open the circuit and run circuit analyses.

Back to top

Can TINA-TI export its circuit to another simulator?
Yes, TINA-TI is PSpice compatible. A Spice netlist created in TINA-TI can run in PSpice.

From the tool's menu, select "File", then "Export", then "Netlist...". A netlist file can be created of a TINA-TI circuit and then run in PSpice.

Back to top

How do I perform parametric analysis?
Step 1: Before running a parametric analysis, add desired components as parametric analysis objects. Click "Analysis" from the menu, then "Select Control Object". Mouse click the selected component, for instance, R2 and see this window:

Click the "..." button, and complete the parametric values from the next window:

Click "OK" after completing the fields in the window. The selected component is set as a parametric analysis object.

Step 2: Run circuit analysis simulation. You will see the circuit performance varies based on the selected parametric object values. See a video on how to perform parametric analysis. (NOTE: Video viewer needed to view example.)

Step 3: You can remove the component as a parametric object after running the parameter analysis by invoking the "parametric stepping" window and clicking the "Remove" button.

Back to top

How can I control the simulation accuracy and speed?
Many factors affect simulation accuracy and speed. Generally, "sharp edge" signals, high error restrictions, or low GMIN will slow the simulation speed. There is a trade-off between simulation accuracy and speed. You can control simulation speed and accuracy balance by adjusting simulation parameters in the program. From the main menu, click "Analysis", then "Set Analysis Parameters...". This window will appear:

As a general rule, this setting can be used. For a circuit working at approximately 100 KHz, set "TR maximum time step" to 100ns. For a switching mode or digital circuit, TR maximum value relative error[%]" to about 1.0% to speed up simulation.

Reducing the value of "Max. no. of saved TR points" will degrade waveform display resolution but will not affect simulation accuracy. However, the simulator will save less data so the analysis waveform will display more quickly.

Click the hand button from the above window to save setting, load previous saved setting, or view the full analysis parameter list.

Back to top

Can I probe a node voltage if I did not use a voltage meter prior to running the simulation?
Yes, by choosing "Save all analysis results" from the "Analysis Options" window. From the menu, select "Analysis", then "Options...". See a video on how to probe signals after simulation. (NOTE: Video viewer needed to view example.)

Back to top

How do I change the simulation progress message mode?
During a simulation, TINA-TI will show the simulation progress status by percentage, message, or detailed information. You can choose one mode from the "Analysis Options" window by clicking "Analysis" from the menu, and then "Option...". In the "General" tab, select from "Trace Mode". See a video on how to choose a simulation progress message bar. (NOTE: Video viewer needed to view example.)

Back to top

Does TINA-TI have a waveform measurement tool?
Yes, TINA-TI can do waveform calculation. Open the "Postprocessing" window by clicking the "add curves" icon on top of the waveform diagram window. Select the kind of function needed and the signals involved. See video on how to do waveform calculation. (NOTE: Video viewer needed to view example.)

Back to top

How do I calculate a loop gain?
There are several ways to calculate a loop gain in TINA-TI, but here is a simple one. See video on how to calculate a loop gain. (NOTE: Video viewer needed to view example.)

Step 1: In the schematic window, inject a voltage source in the feedback loop with a Voltage Generator from the main menu, and set its properties as:

  "Signal" = "Sine wave"
  "IO state" = "None"


Step 2: Place two Voltage Pins at the Voltage Generator terminals - Pin 1 at the positive terminal and Pin 2 at the negative terminal.


Set the Voltage Pin properties as:

   Pin 1: "IO state" = "Output"
   Pin 2: "IO state" = "Input"


   . . . and . . .

Step 3: Run AC simulation. The loop gain from the positive terminal to the negative terminal of the Voltage Generator is calculated and shows the waveform display window.

Back to top

How do I scale waveform in the display window?
From the waveform display window, double-click on one axis to invoke the Set Axis window.


At the bottom of the window, locate the "Round axis scale". The check box controls the signal scale display.

If the check box is unchecked, the tool calculates the scale by the entries of the upper limit, lower limit, and ticks from the Set Axis window with the following formula:

("Upper limit" - "Lower limit")
     "Ticks"

If the check box is checked, the tool sets the scale automatically to rounded numbers and ignores the entries of the upper limit, lower limit, and ticks from the Set Axis window.

For example, when the "Round axis scale" check box is unchecked in the Set Axis window, the waveform will display 7 ticks with upper limit = 86 and lower limit = -82 as they are entered from the Set Axis window:


If the "Round axis scale" check box is checked in the Set Axis window, the waveform will display with rounded numbers and ignore the entries of the uppler limit, lower limit, and ticks from the Set Axis window.

Back to top

Can I use my own device models in TINA-TI?
If you have a Spice model, you can create a macro model for the device and use it in TINA-TI. See the question How do I create a TINA macro model from a netlist (text format) model?".

Back to top

How do I create a TINA macro model from a netlist (text format) model?
TINA's full version can create a macro model from a schematic circuit (*.TSM file) and a netlist circuit (*.CIR file). TINA-TI can only create a macro model from a netlist model (*.CIR file).

Step 1: Create a Spice format sub-circuit netlist file and save as "*.CIR" file. Here is an example of a Spice sub-circuit (for a B340A diode):

subckt b340a 1 2

*... ...

* model content

*... ...
.ENDS

Step 2: Create a macro model with TINA's "New Macro Wizard" from the "Tools" menu.



This will open a dialog box:


Fill in the fields in the above window. In the text box for "Macro Name", enter the macro model's name. It will appear on the schematic when the model is used in a schematic. Enter or navigate to the .CIR file for the macro. You may instead select the “From the Web” option, and use a file directly found on the Internet, for example, from a vendor’s website. When the .CIR file is identified, click “Next” to arrive at the dialog box shown below:

Select the "Load shape from library" button to select a specific symbol from the TINA symbol database (*.DDB files) if it exists. You may then scroll through all of the existing symbols if one applies to your part. You can filter the selections by checking “Show suggested shapes only” or by selecting “Number of pins” and “Shape type”. Or, you can always use the auto-generated symbol for your device by selecting "Auto-generate shape". When you’ve found the symbol you want, click “Next”. You will now be presented with this dialog:

Below the shape, you see pins that are in your macromodel netlist that are unassigned. You then associate those pins with the symbol by clicking on the pin number and dragging it to the pin on the symbol that you want to associate with that pin number. For our example, we’ve connected the pins as shown.

When you click “Next”, you will be presented with a file dialog so you can save the macromodel where you like.

Once saved, you'll see this dialog:

Step 3: Either press the “Insert” button on the last dialog box, or, from the TINA menu anytime, select "Insert", and then "Macro...". Browse to the model file previously saved and place the macro model in the circuit.

Back to top

How do I edit a device model symbol?
A device model symbol is editable by a user after it is placed on a schematic. Right click the mouse when the pointer is on the device symbol, and you will be able to edit it by selecting the edit symbol option.

The modification will only affect the current instance of the model. It has no effect on a new instance of the model from the database.

Back to top

Can I create a TINA library from TINA-TI?
No, the utility is only available in the full version of TINA.

Back to top