CDCE(L)9xx Performance Evaluation Module (Rev. A)
914 views
This user's guide explains how to use the CDCE(L)9xx Performance Evaluation Module (EVM), which is a generic PCB that can handle all the CDCE(L)9xx devices. The CDCE9xx is soldered on the PCB for best performance; therefore, it is necessary to specify the desired device when ordering the EVM. The assembly of the EVM is slightly different for each member of the family. However, the basic functionality remains the same. The CDCE949EVM, CDCE925EVM, and the CDCE913EVM will be available in summer 2007. The CDCEL9xx version will follow later.
|