The TurboTrans software allows the user to determine the T2 module best suited to their design parameters (Vin, Vout, Iout, Ambient Temperature, Airflow) as well as the proper amount of bulk output capacitance required to meet their transient requirements (both using TurboTrans as well as without TurboTrans).
This software will also determine the value of resistor (Rtt) to properly set the TurboTrans to meet the given transient conditions.
Disclaimer
Every effort is made to make this software tool as accurate as possible, but there may be some cases where there are errors. Please double check the specs with the device datasheets before completing your design.
Back to Top