TI is committed to keeping the air clean and safe wherever
we operate by reducing emissions related to our operations,
including manufacturing, transportation and even our landscaping
upkeep. Programs exist to address each of these areas, with
teams dedicated to their management and success.
Programs
NOx and VOC emissions
Maintaining clean air is important at all of our sites globally,
but is perhaps most critical in the Dallas-Fort Worth area.
The area is not in attainment with U.S. ambient air quality
standards for ozone, an air pollutant commonly known as smog.
Smog is formed when nitrous oxides (NOx) and volatile organic
compounds (VOCs) emissions (commonly emitted by cars, lawnmowers
or manufacturing operations) are baked into the atmosphere
during warm months, producing a thick dirty haze that is harmful
to humans, plants and other animals. The region has struggled
for years with developing and implementing an effective plan
that would reduce NOx and VOC emissions and subsequently
improve air quality.
Nearly a decade ago, TI's environmental team took the initiative
to reduce ozone-forming NOx emissions. We have since implemented
a number of air emission and NOx abatement projects. We retrofitted
and replaced manufacturing equipment and upgraded boilers
to reduce emissions. We've also limited generator testing
during peak ozone hours and discouraged the use of combustion
engines (such as lawnmowers) during "ozone action" days.
Likewise, our employee
trip reduction programs have successfully reduced the
number of single-occupancy employee vehicles on the road.
TI has implemented similar programs globally to reduce air
emissions within the communities where we operate.
Evaluating our progress
In 2007, TI successfully implemented a new means of reducing
VOC air emissions from manufacturing operations while also
reducing fuel use and resulting NOx emissions – the first
project of its kind in the industry.
The project began in 2005, when engineers from TI and Matros
Technologies began devising an industry-specific catalyst,
similar to catalytic converters on modern cars, which reduces
harmful emissions. The completed catalyst made it possible
to reduce TI's fuel costs by almost $900,000 a year. More
importantly, the process cut NOx emissions by an estimated
45 percent and will eliminate the disposal of 136 tons of
packing material every four years.
CFC use
In the past, TI used CFCs in our manufacturing and refrigeration
systems, which are critical to our manufacturing and general
operations. CFCs, when released to the atmosphere, have ozone-depleting
properties, which may contribute to global warming and be
harmful to humans and the environment.
In 1989, in support of the Montreal Protocol and in accordance
with the U.S. Clean Air Act, TI developed a standard designed
to phase out the use of Class I ozone depleting substances
(ODSs) worldwide at TI. The rules separately addressed the
use of ODSs in manufacturing and the use of chlorofluorocarbons
(CFCs) used primarily in closed-loop refrigeration systems.
The use of CFCs in manufacturing was eliminated worldwide
by 1993, with the exception of closed system processes such
as process chillers, environmental test chambers and kitchen
refrigeration equipment, which are permissible under the law.
Because CFCs in closed-loop systems leaked very little into
the atmosphere and would have been exceedingly expensive to
replace, we designed a CFC refrigerant recycling program.
The program enabled a gradual phaseout of equipment using
refrigerants.
The recycling program first banned the purchase of CFC-emitting
refrigerants, encouraging instead the reuse of existing equipment
that had been decommissioned. At the time, TI had more than
200 water chillers for large facilities and more than 5,000
pieces of smaller equipment such as kitchen supplies, environmental
test chambers, and drinking fountains.
Back to top
2007 performance
By the end of 2007, TI had reduced the number of large chillers
from 204 to 39 through replacement, retirement, conversion
to alternative refrigerants and the sale of some facilities.
This reduction not only significantly reduced the amount of
CFCs that could be accidentally released to the atmosphere,
but also significantly increased the efficiency of the average
chiller, resulting in less energy consumption and lower operating
costs.
TI's operations in Europe were the first to complete a CFC
elimination program, replacing their last chiller in 2003.
TI Asia is close to completing their program as well, with
only one remaining CFC chiller.
In addition to tracking the number of chillers using CFCs
that remain in the region, TI also strictly monitors the regional
leak rate. Should this leak rate exceed 10 percent, TI enforces
a more stringent set of mitigation requirements.
In 2007, TI's worldwide CFC refrigerant leak rate remained
flat, at less than 3.5 percent.
Back to top |