Corporate Citizenship

Product Stewardship

Environment

Community

Employee Well-being

Advocacy

Corporate Governance

Environment - tree

Water use


Irrigation pond at RFAB facilityWater is one of TI's most valued resources. It is crucial to semiconductor manufacturing, which calls for ultra-clean conditions. It is also critical to the quality of life in the communities where we operate, which is why we work to use this precious resource as efficiently as possible, reducing water use through conservation, reclamation and reuse practices.

Our environmental goal of "zero wasted resources" drives how we plan for and monitor water use, and how efficiently we actually use it. In addition, we identify future water needs, regularly review municipal plans for water use adjustments, and offer our input on reservoir construction and other public infrastructure projects. For example, our Texas sites stay connected with the Texas Water Development Board and its survey activities.

Each TI site maintains a water management program through the site's Environmental, Safety, and Health (ESH) management system, which is at a minimum both OHSAS 18001- and ISO14001-compliant, even if the site has not yet been certified. The Occupational Health and Safety Assessment Series (OHSAS) and International Standardization Organization (ISO) are internationally recognized certification bodies that establish management criteria. Each TI site also monitors its own progress for fair water use and conservation.

Innovative conservation

TI strikes a balance between our own water needs and those of surrounding communities. As a practical consideration, when selecting the location of a new site, TI considers whether the area has sufficient stores of water an important factor. We review both water quality and quantity during site selection, long before beginning construction.

Our water-use innovations have made TI one of the more efficient water users among industry peers. A few examples include:

  • Total water useA deionized water recycling/reuse system installed at our Kuala Lumpur, Malaysia, manufacturing site saved approximately four million gallons of water per month in 2007. That number is projected to increase to 10 million gallons in 2008.
  • The indoor climate-control system at our site in Freising, Germany, pumps cold water from underground aquifers and cycles it through a heating/cooling system, beneficially using the water as a closed-loop heat exchanger. This water is kept separate from all other plant water and processes, which means it is just as clean when it is returned to the aquifer as it was when it was originally extracted.
  • TI Japan strictly adheres to its own zero-impact, zero-industrial discharge policy to preserve certain fish populations, which are prized community assets. Most water at the site is reused, and the rest is used as cooling water for air conditioning facilities.
  • The Central Utility Plant's cooling tower at the North Campus site in Dallas is used to feed building heating and cooling systems, and reuses between 4.5 and 8.5 million gallons per month, depending on the season.
  • In 2007, TI reused about 213 million gallons of water in our North Texas abatement systems alone. These air abatement systems use water to "scrub" manufacturing exhaust.

Back to top

2007 performance

Our manufacturing facilities made progress during the year in improving water efficiency by identifying ways to reduce use and costs through improved tool efficiency and by investing in water conservation systems at sites worldwide.

Despite this progress in 2007, TI's total water use increased 4.7 percent, due to increased production and thus an increase in total water and sewer costs.

Of TI's total water use, we recycled 1.5 billion gallons, or about 19 percent globally, an average of nearly 4 million gallons of water every day. Efficiency measures and conservation practices based on each site's unique characteristics, costs, needs and available financial resources made this possible.

Despite our water conservation efforts, TI's water use at our manufacturing facilities increased in 2007 by about 5.2 percent, a number that takes into account growth and increases in production. Although water use increased 5.2 percent on a per-wafer-shipped basis at our wafer fabrication sites, at TI's assembly and test sites we reduced water use by 6 percent, even though the amount of processing increased 7.9 percent in 2007.

In 2008, TI plans to continue to explore opportunities for reducing water use through conservation and reuse activities.

Back to top

Take a look at TI's social and environmental performance in 2007