|
TI leads the industry in providing digital and analog solutions
with low power consumption and greater energy efficiency.
These innovations enable our customers to meet and exceed
stringent energy guidelines and create new, increasingly
complex applications, such as multi-function cell phones
with long battery life spans and energy-efficient data center
computer servers.
TI’s digital signal controllers and green-mode power supply
controllers enable high-definition televisions (HDTVs) and
other electronics to achieve energy efficiency levels as high
as 90 percent. Our microcontrollers also address efficiency
by reducing energy loss in standby mode. It is estimated
that 5 percent of the electricity used by U.S. homes goes
to objects that absorb and lose energy in standby mode,
such as HDTVs and set-top boxes. That estimate jumps to 12
percent in Japan – equivalent to the output of 18 U.S. power
generation stations. TI’s microcontroller and analog technologies
enable products that consume as little as 500 nanoamps
of electricity in standby mode, consuming less power than a
watch battery.
Our “green” power management chips and digital power
technologies improve the reliability of power supplies by
enabling our customers to design systems that lose less
energy from the power source to the product or device. These
savings result in reduced cooling requirements, extending life
spans, improving reliability through failure prediction and
enabling more precise performance. As a result, TI energyefficient
enabling technologies products are now used in an
array of applications, including server farms, industrial universal
power supplies, alternative energy sources, consumer
electronics like HDTVs and laptops as well as hybrid and
solar-powered vehicles.
TI’s motor control technologies, like digital signal controllers
and analog components, enable customers to use smaller,
more efficient motors. This, in turn, lowers voltages and
produces less heat so that systems can achieve a longer
life and higher reliability. In the U.S., where goods such as
refrigerators consume almost 10 percent of the world’s
electrical power, it is increasingly important that appliances
operate more efficiently.
Using TI’s digital power technology, designers of high-end
servers and telecom infrastructure systems can achieve
greater power efficiency, monitoring and control. The reduced
component count and added intelligence enhances reliability
– an important criterion of power design – and enables
features like failure prediction.
True green energy – clean and renewable power sources like
wind and solar – also benefit from TI’s experience in power
management. For example, TI products are used among
the key electronics solar power systems, including inverters,
which convert electricity from the panels into a usable
household voltage. These high-performance inverters enable
maximum system efficiency during all weather conditions,
including cloudy days.
|