TI unveils details about its 45-nanometer technology
TI’s next-generation manufacturing process will provide customers with early
access to faster, smaller and lower power devices
In advance of the prestigious 2006 Symposia on VLSI Technology and Circuits, Texas Instruments announced details regarding its next-generation process technology. Unveiled just six months after TI initiated volume production of its 65-nanometer chips, the company’s new 45-nm process technology will:

- Increase performance by 30 percent.
- Reduce power consumption by 40 percent.
- Feature TI’s first use of 193-nm immersion photolithography for transistor density improvements that dry lithography is unable to achieve.
- Produce what TI believes to be the smallest 45-nm embedded SRAM memory cells, occupying only 0.24 square microns.
- Feature gate lengths as small as 28 nm.
- Include the use of an ultra-low-k dielectric that achieves a k value of 2.5 and reduces interconnect capacitance by 10 percent.
- Enhance transistor performance and minimize leakage through a collection of strain techniques, including TI’s first use of SiGe induced strain.

TI’s 45-nm semiconductors will be manufactured on 300-mm wafers in the company’s DMOS6 facility in Dallas. The low-power ASIC design library will be available by the end of this year, with samples of the first SoC product delivered in 2007 and initial production in mid-2008.

Links

- Press release announcing TI’s 45-nm technology
- Summary of TI’s keynote paper from the 2006 Symposia
 
    on VLSI Technology and Circuits
- Other TI papers presented at the 2006 Symposia
     on VLSI Technology and Circuits
- Overview of TI’s DMOS6 fabrication facility
- TI sub-100-nm process and manufacturing milestones