Untitled Document
|
|
| Kodak :: CX7530 |
 |
 |
 |
| Zoom Digital Camera |
The EasyShare CX7530 camera was developed
to give people the outstanding picture
quality of a well-designed 5 MP camera
coupled with Kodak’s legendary
ease of operation. The camera incorporates
a Kodak Retinar all-glass, aspherical,
3X optical zoom lens and multi-zone
auto-focus system for crisp prints that
look as od in a frame as they do taped
to the refrigerator. Nine picture modes
are easily accessible, making it simple
to shoot in various situations. The
camera also includes Kodak Color Science
technology to produce realistic, outstanding
pictures even in difficult lighting
conditions, and PictBridge compatibility
for printing without a computer.
The EasyShare CX7530 also includes Kodak’s
new “camera favorites” feature.
With a touch of the red-jeweled Share
button, people can store multiple pictures
in an on-camera digital album. These
pictures can then be shared anytime
on the camera’s large, 1.8-inch,
high-resolution (134,000 pixels) indoor/outdoor
LCD screen. The Share button also allows
someone to immediately select photos
for printing and even e-mailing, with
up to 32 e-mail addresses stored in
the camera’s memory.
For
further information, visit Kodak’s
Web site at www.kodak.com//EasyShare. |
|
|
|
 |
|
|