- TI
DSP Family: The proper and only approved way to refer to
the entire family of TI DSP products is: TMS320 DSP
family.
On first usage, always use the superscript and
generic term DSP following TMS320 when referring to the family.
On second and subsequent uses, you may omit the superscript
, but you must always use the generic term, DSP, following
the TMS320 when referring to the family.
- TI
DSP Platforms: The correct first reference to a TI DSP platform
in text is:
TMS320C6000
DSP platform
TMS320C5000 DSP platform
TMS320C2000 DSP platform
Use either of the following approaches for text variation
on second and subsequent references:
C6000
DSP platform
C5000 DSP platform
C2000 DSP platform
C6000 DSP
C5000 DSP
C2000 DSP
NOTE:
There is no leading apostrophe, which would imply an abbreviation
- TI
DSP Generations: The correct first reference to a TI DSP
Generation is:
TMS320C62x DSP generation
TMS320C67x DSP generation
TMS320C64x DSP generation
TMS320C64x+™ DSP generation
TMS320C5x DSP generation
TMS320C54x DSP generation
TMS320C55x DSP generation
TMS320C20x DSP generation
TMS320C24x DSP generation
TMS320C27x DSP generation
TMS320C28x DSP generation
After first reference, use the following:
C62x
DSP generation
C67x DSP generation
C64x DSP generation
C64x+ DSP generation
C5x DSP generation
C54x DSP generation
C55x DSP generation
C20x DSP generation
C24x DSP generation
C27x DSP generation
C28x DSP generation
On second or subsequent references, use the following:
C62x
DSP
C67x DSP
C64x DSP
C64x+ DSP
C5x DSP
C54x DSP
C55x DSP
C20x DSP
C24x DSP
C27x DSP
C28x DSP
On second or subsequent device references, you may also omit
the trademark designator. However, this relaxation of the
rule applies only at the device level
C62x
DSP
C67x DSP
C64x DSP
C64x+ DSP
C5x DSP
C54x DSP
C55x DSP
C20x DSP
C24x DSP
C27x DSP
C28x DSP
NOTE:
You may use the term "device" in place of "DSP" when referring
to individual products to avoid being overly repetitive. This
does not apply to trademarks for the family, generation or
platform.
- Special
uses:
- When
DSP-related trademarked terms appear in a list, use just
one instance of the generic term, such as "Code Composer
Studio IDE, which is available today on the following
DSP platforms -- C6000, C5000 and the C2000".
- When
using C6000 or C62x in charts, diagrams, schematics,
roadmaps, the platform and device names can be shortened
as long as the title for the piece uses the generic designator
properly, such as TMS320C6000 DSP platform.
- TI
DSP Software: Use the following trademarks for software.
Usage on first reference:
eXpressDSP
Real-Time Software Technology
Code Composer Studio Integrated Development Environment
(IDE)
For text variation, use the following approach for the second
and subsequent references:
eXpressDSP
Software Technology
Code Composer Studio IDE
Or, simply refer to the technology on second or subsequent
references in the following way:
eXpressDSP
Technology
Sample Text: The sample paragraph below provides specific
examples of how to use DSP-related products and services from
TI in product literature, press releases, the web and other
text-based communication tools.
- Example
1: The new TMS320C6000 DSP evaluation module
(EVM) kit from Texas Instruments is the easiest way to begin
development with the world's most powerful line of digital
signal processors, the TMS320 DSP family. The kit,
which is available at a special price of U.S. $199, is a
combination of TI's industry-leading DSP and analog technology,
leading edge development environment and value-added system
expertise. The C6000 DSP EVM -- based on the powerful
TMS320C6201 DSP -- is a complete development environment
that allows OEMs to quickly add their own value-added applications
to the inherent processing power of the C6000 DSP.
Capable of executing more than 1600 million instructions
per second (MIPS), the C6201 DSP is by far the most advanced
DSP available today. Designers in every application area
are already using the device to create next generation products,
such as wireless personal digital assistants (PDAs), remote
wireless terminals and digital subscriber line (DSL) modems
that perform multi-megabits per second (Mbps) speeds.
- Example
2: Software developers can now slash their development
time thanks to eXpressDSP Real-Time Software Technology
with Code Composer Studio Integrated Development Environment
(IDE). Through an advanced toolset and a significant base
of system ready third-party algorithms and tool plug-ins,
eXpressDSP software technology allows real "buy versus
make" decisions for the first time, enabling developers
to concentrate their DSP engineering resources on product
innovation. Real-time kernel services are provided by DSP/BIOS
software, which is enabled by RTDX technology.
- The
DaVinci™ technology trademark
- Always
use the superscript TM immediately after DaVinci before
technology in the first use in all cases
- Technology
should not be capitalized unless it is part of a headline
where all of the words are capitalized.
- To
protect the DaVinci™ trademark, "DaVinci"
must always be followed by a noun that
modifies the goods and services that define DaVinci technology
and may never be used as a possessive.
CORRECT:
DaVinci™ technology is comprised of processors, software
and support...
INCORRECT:
DaVinci™ is comprised of processors, software and support...
(this example doesn't include a noun after "DaVinci")
INCORRECT:
DaVinci’s™ processors enable... (this example
incorrectly uses DaVinci’s ™ as a possessive)
INCORRECT:
The DaVinci™ home page is a resource... (in this example,
"home page" is a noun, but it doesn't modify the
goods and services for DaVinci ™ technology)
INCORRECT:
DaVinci-based chip, processor, technology, platform. etc…
(DaVinci should not be hyphenated, instead should be a processor
based on DaVinci technology)
The
following are examples of possible noun modifiers for DaVinci™:
-
DaVinci™ platform
-
DaVinci™ technology
-
DaVinci™ software
-
DaVinci™ support
-
DaVinci™ development tools
-
DaVinci™ platform of processors
-
DaVinci™ generation of chips
-
DaVinci™ processors
-
DaVinci™ devices
-
DaVinci™ chips
Do
not refer to DaVinci as a single processor, chip or device
since DaVinci technology consists of more than a single device
and this needs to be clear to all audiences.
Part
Numbers and Code Names
- Part
numbers should NOT be identified as a trademark TMS320DM6443/6446
and TMS320DM6431/33/35/37
- On
first reference, ALL part numbers related to devices
based on DaVinci technology should be referenced as follows:
(For example purposes TMS320DM6443 will be used and
all other part numbers should follow the same structure)
CORRECT:
-
TMS320DM6443 DSP based on DaVinci technology (preferred
as this includes the term DSP)
-
TMS320DM6443 digital media processor based on DaVinci technology
-
TMS320DM6443 device based on DaVinci technology
-
TMS320DM6443 processor based on DaVinci technology
INCORRECT:
- DaVinci6443™
device (part numbers are not indicated as a trademark and
DaVinci is the sum of the parts not just a chip)
-
DaVinci processor or DaVinci chip (There are many devices
based on DaVinci technology and no single processor should
be held up as being the DaVinci processor. Do not refer
to processors, chips or devices as a single device.)
Tools
trademarks
- Tools
based on DaVinci technology are not being identified under
the DaVinci trademark.
- First
references to tools should include the full name with the
acronym in parenthesis.
- Never
use DaVinci Evaluation Kit, DaVinci tool.
CORRECT:
The Digital Video Evaluation Module (DVEVM) for DaVinci™
technology provides developers with the ability to write production-ready
application code.
INCORRECT:
The DaVinci™ Evaluation Module provides (No tool includes
DaVinci in the name; all tools are for DaVinci technology.)
Third
Party Network
The
term third party network is not trademarked and there is not
a DaVinci third party network, which is separate from TI’s
DSP Third Party Network.
CORRECT:
DaVinci™ technology is supported by TI’s DSP Third
Party Network …
INCORRECT:
The DaVinci™ third party network. (There is no dedicated
or branded DaVinci third party network.)