| Semiconductor Manufacturing: How a Chip is Made
The semiconductor chip is well recognized today for
the fundamental revolution it brought to the advancement of
electronics technology. Since the first integrated circuit
was created by Jack Kilby in Texas Instruments labs more than 50 years ago, the idea of transistors on silicon becoming
the building blocks for intelligent processors has transformed
almost every facet of daily life. Even though chips are widely
used, how the transformation of simple sand (silicon) into
a highly complex chip occurs is less widely known. This short
description was developed by Texas Instruments to explain
at a high level what takes place in the unique environment
where chips are made, the semiconductor fab.
From Sand to Ingots
The semiconductor manufacturing process begins with
one of the most common elements on earth, silicon. Silicon
is found in abundance in sand, but before it is used in semiconductor
manufacturing it is refined to be virtually 100% pure. Purity
of materials is fundamental to delivering chips that function
as intended.
Pure silicon is then heated until it reaches a molten state
and a perfectly structured silicon “seed” is then
lowered into the molten silicon. The chemical properties of
the molten silicon allow a chemical bond to be formed with
the seed and a long ingot of solid silicon can slowly be pulled
from the silicon as its cools and solidifies around the seed.
When the process is complete, the finished ingot exactly mimics
the physical characteristics of the original seed material.
The ingot is then carefully sawed into thin wafers the diameter
of the ingot, most commonly 200 mm (8-inches) or 300 mm (12-inches)
across.
Into the Fab
TI buys its wafers from companies
that specialize in manufacturing the silicon ingots. Once
the bare wafers, or substrates, arrive at TI, our real work
begins!
Silicon is the base material for chips precisely because of
the conductive properties related to its molecular structure.
Under certain conditions silicon will conduct electricity
and under other conditions it does not. That’s why we
use the term “semiconductor.” This on/off capability
is what underlies the transistor switching action that forms
the ones and zeros of digital logic.
The multiple steps in semiconductor manufacturing all serve
to build components with the necessary electrical structure
to rapidly switch and transfer signals for computational purposes.
In addition to the switching transistors and the metal traces
that conduct electrical signals between various regions of
the chips, insulating materials separate conducting areas
of the device.
In order to alter the characteristics of the semiconductor,
the following steps are undertaken in various sequences depending
on the complexity and functionality of the device.
In between these steps, areas of the chip are patterned
with an image for that particular layer of the device via
photolithography. In photolithography, a very precise “mask”
is used to expose photoresist that has been applied across
the wafer, much like emulsion on film. This pattern hardens
into an exact representation of the mask when it is developed.
Etching then removes selective areas of the pattern using
a plasma that reacts to the material not covered by the hardened
photoresist.
These steps are repeated to create layers of transistors with
precise operating characteristics that have been determined
by the deposition, diffusion and ion implantation steps. A
specialized deposition process called Metallization forms
the critical interconnections between different areas of the
chip and different transistors. Metallization is also used
to form the bonding pads that connect the chip to the package
and then to the circuit board of the system it supports.
After all production steps are complete, a final protective
layer is put over the entire wafer. Probe testing then provides
an initial look at how many functional devices are on the
wafer. (Current technology allows us to pack more than 180,000 transistors in the cross-sectional area of a single
human hair. At such tiny dimensions, even the smallest dust
particle can ruin the functionality of an entire chip!) Next,
a very precise saw cuts the individual chips from the wafer
and the good die are packaged, tested again and shipped to
the customer.
Although the above steps are in general use across the semiconductor
industry, proficiency in manufacturing is a vital aspect to success in
this highly competitive market.
|