Industry Associations

TI is a member of the following trade associations.

United States

International

TI paid a total of $1,666,531.00 in dues to the above organizations in 2017. These organizations either received $5,000 or more in dues or are involved in lobbying activities or both. The portion of those dues used for lobbying and/or political activities that are nondeductible under Section 162 (e) (1) of the Internal Revenue Code amounted to $348,414.00.