Texas Instruments Technology for Innovators
TI Public Affairs Report  
  Government

Imagine – every year our country welcomes the best and brightest students from around the world to study at our universities. Then, shortly after graduation, or perhaps a few years after working for a U.S.-based company like Texas Instruments, we send them back overseas to work for foreign competitors. This is the effect our broken immigration system has on highly educated foreign nationals.

Despite the many controversial issues involved in immigration reform, one thing is clear: for the U.S. to remain competitive, our companies need to be able to hire and retain the brightest minds in the world, especially graduates from our universities.

The semiconductor industry depends on electrical engineers to continually innovate in the design and development of new chips. In 2006, U.S. universities awarded more than half of their master’s degrees and 71 percent of their Ph.D.s in electrical engineering to foreign nationals. At some campuses in Texas, these figures are even higher (see Table 1). TI and other high-tech employers need predictable access to this talent.

Although TI continues to hire only a small number of foreign professionals each year, they are typically important contributors and have the talents we seek to retain in long-term employees. Indeed, if you look at some of our top business managers and technologists in the company, many are foreign-born. They help drive business that supports thousands of TIers as well as numerous suppliers and downstream businesses in Texas and the U.S.

It is counterproductive for this country to train and employ foreign scientists and engineers and then send them home with the skills and know-how to compete against American businesses. Even worse is to lose employees who have worked for our company for several years but eventually leave out of frustration over waiting for a visa. Although we continue to try to increase the pipeline of domestic students in these disciplines – and TI is doing its part to help address that need – we must be able to hire and retain foreign students and professionals.

The shortage of H-1B visas is well documented, as illustrated by hitting the 2008 cap of 65,000 within the first two days as companies scrambled to get their share of a pie that is too small. A lesser-known side of the same coin is the shortage of employment-based permanent resident visas, or green cards.

Long waits for green cards have become an urgent problem for hundreds of TI employees. These highly educated professionals face at least a five- to seven-year wait, leaving them in personal and professional limbo and limiting their promotion and mobility options. These waits are largely caused by insufficient numbers of green cards, which are set by law.

The immigration bill introduced in the U.S. Senate falls short of the relief sought by TI and others in the high-tech community, particularly with respect to the numbers of green cards and H-1B visas for highly educated professionals and a predictable implementation of a new merit-based system.

Sen. John Cornyn (R-Texas), together with Sen. Maria Cantwell (D-Wash.) introduced an important amendment to address the concerns of high-tech employers. Sen. Kay Bailey Hutchison (D-Texas) was also supportive of the proposal. On June 7, before these issues could be resolved, the Senate failed to invoke cloture on the bill for the third time, a procedural mechanism that limits debate and guarantees an eventual vote. Senate Majority Leader Harry Reid (D-Nev.) decided to put the bill on hold.

On June 11, Sen. Reid and Minority Leader Mitch McConnell (R-Ky.) announced that the Senate would return to the bill before the July 4 recess. The Cantwell-Cornyn amendment has been superseded by the Kyl-Cantwell amendment, which would expand the H-1B cap to 180,000, double the H-1B advanced degree exemption from 20,000 to 40,000 and phase in the merit system by reserving green card visas for employers. Although the proposal falls short of adding the needed green card numbers, it represents an improvement over the bill as introduced.

TI and others in the high-tech community will continue to advocate for meaningful immigration reform for highly educated professionals and remain hopeful that the process can move forward in Congress. Our country’s innovation leadership depends on it.

Table 1 – 2006 degrees granted in Texas to foreign nationals in electrical engineering.

 

Master’s Degrees

Ph.D.s

Rice

40%

75%

UT Austin

41%

75%

UT Dallas

70%

89%

Texas A&M

68%

88%

Texas Tech

50%

40%


Products  |  Applications  |  Support  |  Site Map
© Copyright 1995-2008 Texas Instruments Incorporated. All rights reserved. Trademarks  |  Privacy Policy  |  Terms of Use