To ensure delivery to your inbox, please add tiprime@dlep14.itg.ti.com to your address book or safe sender list.

MSP430 Newsflash 1Q 2008     www.ti.com/msp430      Subscribe
   
Product Announcements    Literature & App Notes    University News    
 Third Party News    Features    Training/Seminars    TI Products to Use With MSP430
   
  Product Announcements
MSP430F261x/MSP430F241x

64-/80-Pin High-End F16x/14x Upgrade
The 261x and 241x serve as a high-end pin and function-compatible migration path for customers using the 64-pin F16x and F14x families. On-chip memory has doubled to 120 kB, GPIO pin count is now 64 and performance has increased to 16 MIPS. In addition, there is 8 KB of RAM, 12-bit 200 kSPS ADC (two),
12-bit DAC, (two) USCI, DMA, MPY timer_A3/B7 and WDT+. These devices are compatible in price with their predecessors, the F16x and F14x.

Applications: Sensor systems, industrial control applications, handheld meters
Package: 64-pin LQFP/TQFP, 80-pin LQFP
Recommended Development Tools:
MSP-FET430U64, MSP-FET430U80



MSP430F21x2

Coming in April 2008!
Built-in 16-bit timers, a fast 10-bit A/D converter with integrated reference and a data transfer controller (DTC), a comparator and built-in communication capability that uses USCI, and up to 24 I/O pins.

Applications: Smoke detectors, battery chargers, wireless security, wireless sensors
Package: 28-pin TSSOP, 32-pin QFN
Recommended Development Tools:
MSP-FET430U28

  Literature & App Notes
New MSP430 App Notes
PMBus Implementation using the MSP430 USCI Abstract
MSP430 Capacitive Single-Touch Sensor Design Guide Abstract
CEC-to-I²C Bridge with the MSP430 Abstract
Extended Memory Access Using IAR v3.42A and CCE v2 Abstract
Migrating from MSP430F16x to MSP430F261x Abstract
Migrating from MSP430F13x/14x to MSP430F23x/24x Abstract

  University News
MSP430 and Connexions
Earn a Free eZ430-RF2500 Tool! Contribute Content to Connexions

TI would like your help in spreading knowledge about MSP430 devices by contributing a content module of unique information to Connexions. All you have to do is go to Connexions and create an account and a module, then submit the content using the form at the Web site below. Modules include everything from basic explanations of microcontroller architecture to student design projects and common MSP430 uses, plus complete course lessons and lab setups. See www.ti.com/msp430connexions to learn how your module can earn you a FREE eZ430-RF2500 development tool.

  Third Party News

VishayAMB2520
Add infrared communication to your device by choosing Vishay’s Courier-115 wireless solution.  The proven, royalty-free software protocol allows you to focus on your product development, knowing the wireless feature is ready to go.  The software code is small: ~2 kbyte of ROM.  Infrared is an unregulated medium requiring no UL or CE compliance testing. As a leader in infrared communication, Vishay offers transceivers in a variety of package sizes and transmit distances.  Ideal for data logger and metering applications like.
Uploading data from the data logger to the host
Downloading firmware from the host to the data logger or meter
Calibrating and setting parameters during manufacturing

For more info, email courier115@vishay.com



PassWorldPentad Design

PassWorld YK has designed a low-profile development kit based on MSP430F169 (F1611 is in production right now). This board features a 101x64 pixel graphic display, a real-time clock with backup power, an SD card and a navigation switch. This board can be expanded using 1.27mm universal PCB for your experiments. This means that one development kit can be used for several prototypes just by changing the extension board. PassWorld also provides C-source code that shows how to use the different parts of the board. Other libraries (e.g., FAT file system and UNICODE Japanese characters) are also available on demand.

  Features
430 Day 2008
Free three-hour lunch-and-learn
You will get an MSP430 architecture overview, information on future generations, wireless applications and technical demonstrations
Register and attend to get your FREE eZ430-RF2500 low-power wireless development tool ($49 value)
Starts March 27, 2008
Register today!

  Training/Seminars
Sign Up for ZigBee® Training
The Low-Power RF and ZigBee Networking Workshop is the best way to get on the fast track to ZigBee success. This hands-on, three-day course will furnish a solid foundation in RF capabilities, MAC layer communications, OSAL/HAL usage, ZigBee networking and Z-Stack™-based product development. The class is taught by an experienced engineer and provides information, techniques and strategies you will not find elsewhere. Even if you are currently just evaluating ZigBee, our training course is designed to get you started the right way.

Upcoming trainings:

USA
March 11   San Jose, Calif.
April 15     Waltham, Mass.

Europe
March 11   Landshut, Germany
More

  TI Products to Use With MSP430
The RF360, the smallest smart IC platform in the market, will integrate TI’s ultra-low-power MSP430 microcontroller, advanced embedded Ferroelectric Random Access Memory (FRAM) and high-performance RF Analog Front-End (AFE) technologies. Leveraging a low-power architecture and enhanced write capability, the RF360 smart IC platform will offer fast chip transaction speeds that will enable governments to quickly and efficiently produce a multitude of passive electronic identification (ID), such as electronic passports (e-passports) and national ID cards. (See www.ti.com/govid.)

Ultra-low-power architecture is critical to passive (non-battery) contactless applications, such as national IDs and e-passports. With the MSP430 microcontroller as an integral component of the RF360 technology architecture, government ID customers can leverage the world’s most power-efficient microcontroller, which is used in hundreds of low-power mobile products. The MSP430’s reduced instruction set significantly decreases the size of its software code compared to other microcontrollers on the market, driving faster transaction times and lower-power consumption.

TI’s RF360 employs an advanced embedded memory technology called FRAM, which improves the speed and reliability of future smart, secure e-passports and government ID documents. The technology produces a significant improvement over the non-volatile memory technologies used in current electronic government ID, such as Electrically Erasable Programmable Read-Only Memory (EEPROM) and Flash. The technology also offers major advantages in terms of transaction speed, power consumption and enhanced write data reliability.

For more information on how the RF360 platform leverages the advantages of embedded FRAM, please download “The Advantages of FRAM-Based Smart ICs for Next-Generation Government Electronic IDs” at www.ti.com/govidwp.

The platform bar and Z-Stack are trademarks of Texas Instruments. ZigBee is a registered trademark of ZigBee Alliance. All other trademarks are the property of their respective owners.

%%DYN_FOOTER%%