TI Public Affairs Report
Texas Instruments
  Environment
EPA recognizes TI with Clean Air Excellence Award

TI was among 11 winners named to receive the U.S. Environmental Protection Agency's eighth annual Clean Air Excellence Awards for outstanding accomplishments in improving air quality and reducing greenhouse gas emissions. The awards were presented recently at a ceremony in Washington, D.C.

There are four categories of awards: clean air technology, community action, education/outreach, and regulatory policy innovations. TI and Matros Technologies Inc. (MT) were recognized for innovative clean air technology they developed jointly, which improves the abatement of volatile organic compounds (VOCs) in semiconductor manufacturing.

"This year's Clean Air Excellence Award winners' dedication to creating a cleaner tomorrow is truly a breath of fresh air," said EPA Administrator Stephen L. Johnson. "From local to state governments, companies to citizen groups, these award winners are helping the EPA deliver healthier air and healthier lives to all Americans."

TI and MT initially collaborated to reduce emissions at three of TI's semiconductor manufacturing facilities. As a result of their joint research and development, the companies discovered added environmental benefits.

The installation of the Matros copper-chromium catalyst reduced nitrogen oxide emissions and improved VOC performance. The catalyst installation made it possible to oxidize VOCs at lower temperatures.

Due to the lower oxidation temperature, the process uses 50 to 60 percent less fuel and cuts nitrogen oxide emissions by 40 percent. The new process also eliminates the disposal of 136 tons of packing materials every four years. Finally, using MT's catalyst, more than 99 percent destruction efficiency is possible, improving energy recuperations and reducing maintenance activities.

This technology reduces the use of natural gas as well as materials and labor and disposal costs. The TI and MT collaboration has successfully reduced air emissions and material disposal at TI and can be applied globally to similar facilities in the industry.

The Clean Air Excellence Awards recognize and honor outstanding, innovative efforts that make progress in achieving cleaner air. The awards were established in 2000, at the recommendation of the Clean Air Act Advisory Committee, a senior-level policy group that advises the EPA on implementing the Clean Air Act. For a complete list of this year's EPA award winners nationwide, see http://www.epa.gov/air/caaac/recipients.html


Products  |  Applications  |  Support  |  Site Map
© Copyright 1995-2008 Texas Instruments Incorporated. All rights reserved. Trademarks  |  Privacy Policy  |  Terms of Use