ELM

In the case of NAND modules with no internal correction capability, sometimes referred to as bare NAND, the correction process can be delegated to the error location module (ELM) used in conjunction with the GPMC.

The ELM supports the following features:

  • 4, 8, and 16 bits per 512-byte block error location based on BCH algorithm
  • Eight simultaneous processing contexts
  • Page-based and continuous modes
  • Interrupt generation when error location process completes:
    • When the full page has been processed in page mode
    • For each syndrome polynomial (checksum-like information) in continuous mode

For more information, see section Error Location Module (ELM) in chapter Memory Subsystem of the Device TRM.