Timers

The device has 16 general-purpose (GP) timers (TIMER1 - TIMER16), two watchdog timers, and a 32-kHz synchronized timer (COUNTER_32K) that have the following features:

  • Dedicated input trigger for capture mode and dedicated output trigger/pulse width modulation (PWM) signal
  • Interrupts generated on overflow, compare, and capture
  • Free-running 32-bit upward counter
  • Supported modes:
    • Compare and capture modes
    • Auto-reload mode
    • Start-stop mode
  • On-the-fly read/write register (while counting)

The device has two system watchdog timer (WD_TIMER1 and WD_TIMER2) that have the following features:

  • Free-running 32-bit upward counter
  • On-the-fly read/write register (while counting)
  • Reset upon occurrence of a timer overflow condition

The device includes one instance of the 32-bit watchdog timer: WD_TIMER2, also called the MPU watchdog timer.

The watchdog timer is used to provide a recovery mechanism for the device in the event of a fault condition, such as a non-exiting code loop.

In are presented the specific groupings of signals (IOSET) for use with TIMERS.

NOTE

For additional information on the Timer Module, see the Device TRM.