SLOS866F May 2014 – March 2018 DRV2604L
PRODUCTION DATA.
In the active state, the DRV2604L device has I2C communication and is capable of playing waveforms, running calibration, and running diagnostics. These operations are referred to as processes. Figure 17 shows the flow of starting, or firing, a process. Notice that the GO signal fires the processes. Note that the GO signal is not the same as the GO bit. Figure 18 shows a diagram of the GO-signal behavior.
NOTE:
If an output short is present before a waveform is played, changing modes (with the MODE[2:0] bit in register 0x01) is required to resume normal playback.