SCES215Y April 1999 – December 2017 SN74LVC1GU04
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The unbuffered inverter is commonly used in oscillator circuits because it is less sensitive to parameter changes in the oscillator circuit due to having lower total gain than a buffered equivalent. An example application circuit is shown in Figure 5. To learn more about how to use an unbuffered inverter in an oscillator circuit, refer to the Use of the CMOS Unbuffered Inverter in Oscillator Circuits application report.
This device uses CMOS technology and has balanced output drive. Take care to avoid bus contention because it can drive currents that would exceed maximum limits. The high drive also creates fast edges into light loads, so routing and load conditions should be considered to prevent ringing.
To learn more about how to use an unbuffered inverter in an oscillator circuit, refer to the Use of the CMOS Unbuffered Inverter in Oscillator Circuits application report.