JAJSEF1D December 2013 – December 2021 DAC7750 , DAC8750
PRODUCTION DATA
The second method to implement HART is to couple the HART signal through the ISET-R pin when IOUT is operated using an external RSET resistor. The FSK signal from the modem is ac-coupled into the pin through a series combination of Rin and Cin as shown in Figure 9-2.
The magnitude of the ac-current output is calculated with Equation 6.
where
The series input resistor and capacitor form a high-pass filter at the ISET-R pin. Select Cin to make sure that all signals in the HART extended-frequency band pass through unattenuated.