Open main.syscfg file by double-clicking on the filename in the Project window. Under the Project Options, select Closed Current Loop as the INCR_BUILD option. Select Single-phase PFC and the valley switching option should be automatically set to valley switching enabled. Save the main.syscfg file. Rebuild the whole project to make the change happen. This is shown in Figure 20.
Open solution_settings.h file. Notice that the incremental build (INCR_BUILD) option is set to "1" (Build 2) and INTERLEAVE option is set to "1" (valley switching control is enabled).
If another build option was built previously, right click on the project name and click on Clean Project. Click Project → Build All button and watch the tools run in the build window.
"Turn on" the 12-V DC bench power supply. Click the Debug button or click Run → Debug from the menu. Once complete, the Build 2 code should compile and load.
Notice the CCS Debug icon in the upper right corner, indicating that the user in now in the Debug Perspective view. The program should be stopped at the start of main().