Open main.cfg file by double-clicking the filename in the Project window. Under Project Options, select Closed Current Loop & Closed Voltage Loop as the INCR_BUILD option. Select the Single phase PFC and the valley switching options should be automatically set to valley switching enabled as shown in Figure 28. Save the main.cfg file. Rebuild the project if there are any changes in solution_settings.h.
Open solution_settings.h file. Notice that the incremental build (INCR_BUILD) option is set to"3" and the INTERLEAVE option is set to "1" (valley switching control is enabled).
If another build option was built previously, right click the project name and then click Clean Project. Click Project → Build All button and watch the tools run in the build window.
Turn on the 12-V DC bench power supply. Click the Debug button or click Run → Debug. The build 3 code should compile and load.
Notice the CCS Debug icon in the upper right-hand corner, which indicates the Debug Perspective view. The program should be stopped at the start of main().