JAJU787B April 2016 – May 2019 TPS2828 , TPS3828
The example project can be built with CCS IDE v9.0.1 (or above). The two CCS projects of HybridRfPlcExample_CC1310_LAUNCHXL_tirtos_ccs and tirtos_builds_CC1310_LAUNCHXL_release_ccs need to be opened to compile the project. The screen capture of the project view is shown in Figure 16. Once successfully compiled, the binary file (HybridRfPlcExample_CC1310_LAUNCHXL_tirtos_ccs.out) will be generated in the directory of debug.