SLVAEV0A July   2020  – July 2022 TPS25833-Q1

 

  1.   Trademarks
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)
  6. 5Revision History

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the TPS25833-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to supply (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
Class Failure Effects
A Potential device damage that affects functionality.
B No device damage, but loss of functionality.
C No device damage, but performance degradation.
D No device damage, no impact to functionality or performance.

Figure 4-1 and Figure 4-2 show the TPS25833-Q1 pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TPS25833-Q1 data sheet.

GUID-20210719-CA0I-ZMDV-LD7C-9B23W7ZBZLD6-low.gif Figure 4-1 TPS25833QCWRHBRQ1 Pin Diagram
GUID-A921DCE6-4824-4B8E-9BC1-B6DF8C2E9480-low.gif Figure 4-2 TPS25833QWRHBRQ1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • Device used within the 'Recommended Operating Conditions' and the 'Absolute Maximum Ratings' found in the appropriate device data sheet.

  • Configuration as shown in the 'Example Application Circuit' found in the appropriate device data sheet.

Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
VIN 1 Device does not operate. No output voltage is generated. B
VIN 2 Device does not operate. No output voltage is generated. B
VIN 3 Device does not operate. No output voltage is generated. B
EN 4 Loss of ENABLE functionality. Device remains in shutdown mode. B
CTRL1 5 Device stays at reserved mode or DCP auto mode. When in the reserved mode, the output charging is abnormal. B
CTRL2 6 Device stay at reserved mode or SDP mode. When in the reserved mode, the output charging is abnormal. B
/THERM_WARN 7 Loss of THERM_WARN functionality. Device always appears to be in the thermal warning condition. C
NTC 8 Loss of Temperature Sense functionality. Device cannot sense the external PCB temperature. C
RT/SYNC 9 Device internal buck switching frequency goes up to 4.6 MHz, and the CSN pin voltage up to 7 V. It makes the output charging. B
LS_GD 10 Device cannot drive external FET for current limit. B
IMON 11 Loss of Cable Compensation functionality. Device cannot make a cable compensation. C
ILIMT 12 Loss of Current Limit functionality. Device uses the maximum current limit value of 3.5 A. C
CSN/OUT 13 Device internal buck output short circuits. Device enters hiccup mode. B
CSP 14 Device internal buck output short circuits. Device enters hiccup mode. B
BUS 15 Device hiccups and output current limit does work. B
AGND 16 No effect D
DM_IN 17 Device cannot support SDP/CDP/DCP auto charging mode. B
DP_IN 18 Device cannot support SDP/CDP/DCP auto charging mode. B
CC2 19 Device hiccups and output voltage is abnormal. B
CC1 20 Device hiccups and output voltage is abnormal. B
VCC 21 Device hiccups and cannot be powered on. B
/POL 22 Loss of /POL functionality. Device always appears to the CC2 pin is connected to the CC line in the cable. C
/LD_DET 23 Loss of /LD_DET functionality. Device always appears to a Type-C UFP is identified on the CC lines. C
/FAULT 24 Loss of /FAULT functionality. Device always appears to be in the fault condition. C
PGND 25 No effect D
PGND 26 No effect D
PGND 27 No effect D
SW 28 Device internal buck hiccup. Long-term reliability can impact. A
SW 29 Device internal buck hiccup. Long-term reliability can impact. A
SW 30 Device internal buck hiccup. Long-term reliability can impact. A
SW 31 Device internal buck hiccup. Long-term reliability can impact. A
BOOT 32 Device internal buck stop switching. No output voltage in VSN/OUT. B
Thermal Pad No effect D
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
VIN 1 Long-term reliability can impact due to lower bonding-wire count. C
VIN 2 Long-term reliability can impact due to lower bonding-wire count. C
VIN 3 Long-term reliability can impact due to lower bonding-wire count. C
EN 4 Device off and on cannot be controlled and is off and on depending on how EN floats. B
CTRL1 5 Device DCP auto/SDP/CDP/RESERVED mode cannot be controlled, and is DCP auto/SDP/CDP/RESERVED mode depending on how CTRL1 floats. B
CTRL2 6 Device DCP auto/SDP/CDP/RESERVED mode cannot be controlled, and is DCP auto/SDP/CDP/RESERVED mode depending on how CTRL2 floats. B
/THERM_WARN 7 Loss of THERM_WARN functionality. Device cannot be determined whether it is in the overtemperature condition. C
NTC 8 Device overtemperature or not cannot be controlled, and is depending on how NTC floats. C
RT/SYNC 9 Device internal buck switching frequency drop and loading current are limited to about a small value. This fact causes abnormal charging. B
LS_GD 10 Device cannot drive external FET for current limit. B
IMON 11 VOUT/CSN goes up to 6.9 V. This action can cause VBUS voltage over compensation and fail at the BC1.2 certification test. B
ILIMT 12 Device internal buck hiccups. B
CSN/OUT 13 Device internal buck output voltage is abnormal. B
CSP 14 Device cannot sense the output current signal. The output current limit and VBUS cable compensation don not work. C
BUS 15 Loss of VBUS OVP functionality. IEC ESD test is impacted. B
AGND 16 The device tries to power up by forward-biasing the ESD diode from the GND to another pin. Strange results are observed. B
DM_IN 17 Device cannot support SDP/CDP/DCP auto charging mode. B
DP_IN 18 Device cannot support SDP/CDP/DCP auto charging mode. B
CC2 19 Device Nothing attached/UFP connected/No UFP connected cannot be controlled. It depends on the state of CC1. B
CC1 20 Device Nothing attached/UFP connected/No UFP connected cannot be controlled. It depends on the state of CC2. B
VCC 21 Device cannot start up. Internal buck stops switching. B
/POL 22 Loss of /POL functionality, cannot give cable orientation information. C
/LD_DET 23 Loss of /LD_DET functionality. Cannot identify the Type-C UFP. C
/FAULT 24 Loss of /FAULT functionality, cannot check whether the device is in the fault condition. C
PGND 25 Long-term reliability can impact due to lower bonding-wire count. C
PGND 26 Long-term reliability can impact due to lower bonding-wire count. C
PGND 27 Long-term reliability can impact due to lower bonding-wire count. C
SW 28 Long-term reliability can impact due to lower bonding-wire count. C
SW 29 Long-term reliability can impact due to lower bonding-wire count. C
SW 30 Long-term reliability can impact due to lower bonding-wire count. C
SW 31 Long-term reliability can impact due to lower bonding-wire count. C
BOOT 32 Device internal buck HS FET cannot be turned on. VSN/OUT cannot get up to target voltage. B
Thermal Pad Long-term reliability can impact if the device operates beyond the rate junction temperature for extended time because a heat path is interrupted. C
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effect(s) Failure Effect Class
VIN 1 VIN No effect D
VIN 2 VIN No effect D
VIN 3 EN Device is enabled and cannot be disabled. D
EN 4 CTRL1 Device DCP auto/SDP/CDP/reserve mode and enable/disable cannot be controlled. It is DCP auto/SDP/CDP/ reserve mode and enable/disable depending on how EN and CTRL1 circuits interact. B
CTRL1 5 CTRL2 Device DCP auto/SDP/CDP/Reserve mode cannot be controlled. It is DCP auto/SDP/CDP/Reserve mode depending on how CTRL1 and CTRL2 circuits interact. B
CTRL2 6 /THERM_WARN Device DCP auto/SDP/CDP/Reserve mode cannot be controlled. It is DCP auto/SDP/CDP/Reserve mode depending on how CTRL2 and /THERM_WARN circuits interact. B
/THERM_WARN 7 NTC The NTC thermal sensing does not work, THERM_WARN flag and charging state do not report correctly. B
NTC 8 RT/SYNC Device internal buck switching is interrupted by NTC. B
RT/SYNC 9 LS_GD The LS_GD goes down from 11.3 V to 0.5 V, and the internal buck switching frequency is abnormal. Device cannot drive the external FET for current limit B
LS_GD 10 IMON LS_GD voltage set low, device cannot drive the external FET for current limit. B
IMON 11 ILIMT Current limit threshold and cable compensation value are impacted. C
ILIMT 12 CSN/OUT Ilimit is pulled up over 1 V, device behaves as average current limit and keeps hiccup. B
CSN/OUT 13 CSP Average current limit, external FET current limit and cable compensation function are bypassed. C
CSP 14 BUS Average current limit, external FET current limit and cable compensation function are bypassed. C
BUS 15 AGND Device goes into hiccup mode. B
AGND 16 DM_IN Device cannot support SDP/CDP/DCP auto charging mode. B
DM_IN 17 DP_IN Device only supports BC1.2 DCP mode. C
DP_IN 18 CC2 If shorted before charging, the device cannot charge. If shorted after charge, no effect. B
CC2 19 CC1 Pin short before power up, device internal buck is not switching. Pin short during normal condition, no impact. B
CC1 20 VCC Device stops working, CSN/OUT does not output voltage. B
VCC 21 /POL Loss of /POL functionality, the /POL always goes into high, device always appears to have the CC1 pin connected to the CC line. C
/POL 22 /LD_DET Loss of /POL and /LD_LET functionality. C
/LD_DET 23 /FAULT Loss of /FAULT and /LD_LET functionality. C
/FAULT 24 PGND Loss of /FAULT functionality, device always appears to be in the fault condition. C
PGND 25 PGND No effect D
PGND 26 PGND No effect D
PGND 27 SW Device internal buck hiccup, long-term reliability can be impacted. A
SW 28 SW No effect D
SW 29 SW No effect D
SW 30 SW No effect D
SW 31 BOOT Device internal buck HS FET stops working, no output voltage in CSN/OUT. B
Thermal Pad Any of the numbered pins in the above rows. The thermal pad is connected to the board ground. Treat shorts to the thermal pad as shorts to ground. A
Table 4-5 Pin FMA for Device Pins Short-Circuited to Supply
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
VIN 1 No effect D
VIN 2 No effect D
VIN 3 No effect D
EN 4 Device is enabled and cannot be disabled. D
CTRL1 5 Above ABS voltage, device can be damaged. A
CTRL2 6 Above ABS voltage, device can be damaged. A
/THERM_WARN 7 Above ABS voltage, device can be damaged. A
NTC 8 Above ABS voltage, device can be damaged. A
RT/SYNC 9 Above ABS voltage, device can be damaged. A
LS_GD 10 External FET cannot do current limit. C
IMON 11 Above ABS voltage, device can be damaged. A
ILIMT 12 Above ABS voltage, device can be damaged. A
CSN/OUT 13 VBUS OVP protection. FAULT pin asserts. B
CSP 14 VBUS OVP protection. FAULT pin asserts. B
BUS 15 VBUS OVP protection. FAULT pin asserts. B
AGND 16 Former power supply can be pulled down. Device is not powered up. B
DM_IN 17 Above ABS voltage, device can be damaged. A
DP_IN 18 Above ABS voltage, device can be damaged. A
CC2 19 Above ABS voltage, device can be damaged. A
CC1 20 Above ABS voltage, device can be damaged. A
VCC 21 Device broken, VCC pin voltage exceeds the ABS maximum value. A
/POL 22 Above ABS voltage, device can be damaged. A
/LD_DET 23 Above ABS voltage, device can be damaged. A
/FAULT 24 Above ABS voltage, device can be damaged. A
PGND 25 Former power supply can be pulled down. Device is not powered up. B
PGND 26 Former power supply can be pulled down. Device is not powered up. B
PGND 27 Former power supply can be pulled down. Device is not powered up. B
SW 28 Device internal buck stops working. B
SW 29 Device internal buck stops working. B
SW 30 Device internal buck stops working. B
SW 31 Device internal buck stops working. B
BOOT 32 Above ABS voltage, device can be damaged. A
Thermal Pad Thermal pad is connected to PGND on the PCB board. Former power supply can be pulled down. Device is not powered up. B