SPRAB89B September 2011 – August 2025
Interrupts, hardware exceptions, and OS signals cannot be handled directly by exceptions.
Because interrupt functions could happen anywhere, we cannot support propagating exceptions from interrupt functions. All interrupt functions will be EXIDX_CANTUNWIND. However, interrupt functions can call functions which might themselves throw exceptions, and thus interrupt functions must be in the EXIDX table and may have descriptors, but will never have unwinding instructions.
Applications which wish to use an exception to represent interrupts must arrange for the interrupt to be caught with an interrupt function, which must set a global volatile object to indicate that the interrupt has occurred, and then use the value of that variable to throw an exception after the interrupt function has returned.
If an OS provides signal, exceptions representing signals must be handled similarly.