SPRAB89B September 2011 – August 2025
Figure 1-1 shows the components of the ABI and their relationship. We will briefly describe the components, beginning with the lower part of the diagram and moving upward, and provide references to the appropriate chapter of this ABI specification.
The components in the bottom area relate to object-level interoperability.
Figure 1-1 Parts of the ABI
SpecificationThe C Language ABI (Chapter 2, Chapter 3, Chapter 4, Chapter 5, Chapter 8 and Chapter 9) specifies function calling conventions, data type representations, addressing conventions, and the interface to the C run-time library.
The C++ ABI (Chapter 10) specifies how the C++ language is implemented; this includes details about virtual function tables, name mangling, how constructors are called, and the exception handling mechanism (Chapter 11). The C6000 C++ ABI is based on the prevalent IA-64 (Itanium) C++ ABI.
The DWARF component (Chapter 12) specifies the representation of object-level debug information. The base standard is the DWARF3 standard. This specification details processor-specific extensions.
The ELF component (Chapter 13) specifies the representation of object files. This specification extends the System V ABI specification with processor specific information.
Build Attributes (Chapter 17) refer to a means of encoding into an object file various parameters that affect inter-object compatibility, such as target device assumptions, memory models, or ABI variants. Toolchains can use build attributes to prevent incompatible object files from being combined or loaded.
The components in the central area of the diagram relate to execution-time interoperability. The dynamic linking components (Chapter 6 and Section 14.3) specify a mechanism whereby separately linked modules can interoperate, including the sharing of their code. Part of the dynamic linking mechanism is a method for data addressing such that separately linked modules can address each other's data without relocation.
Thread-Local Storage (Chapter 7) allows for the creation of thread-specific variables with static storage duration. The specification, representation, and access of thread-local variables is described in this document.
Symbol versioning (Chapter 16) is a mechanism whereby symbolic references include a minimum version, such that they are dynamically resolved with definitions having at least that version, in order to prevent run-time incompatibilities. This ABI adopts the standard GCC/Linux model, with no changes.
The components in the top part of Figure 1-1 augment the ABI with platform-specific conventions that define the requirements for executables to be compatible with an execution environment, such as the number and use of program segments, addressing conventions, visibility conventions, pre-emption, program loading, and initialization. Bare-Metal refers to the absence of any specific environment. The only other environment currently covered by the ABI is the Linux platform (Chapter 15).
Finally, there is a set of specifications that are not formally part of the ABI but are documented here both for reference and so that other toolchains can optionally implement them.
Initialization (Chapter 18) refers to the mechanism whereby initialized variables obtain their initial value. Nominally these variables reside in the .data section and they are initialized directly when the .data section is loaded, requiring no additional participation from the tools. However the TI toolchain supports a mechanism whereby the .data section is encoded into the object file in compressed form, and decompressed at startup time. This is a special use of a general mechanism that programmatically copies compressed code or data from offline storage (e.g. ROM) to its execution address. We refer to this facility as copy tables. While not part of the ABI, the initialization and copy table mechanism is documented here so that other toolchains can support it if desired.
Program Header Attributes (Chapter 19) are an extension to ELF implemented by the TI toolchain in order to represent various additional properties of ELF segments beyond what is specified by the base ELF standard. The TI tools use them to encode memory connectivity/latency requirements, protection, cache behavior, and other system-specific properties. They are designed to be flexible and extensible. Again, we document them here so that other tools can interoperate with them if needed.