SPRAB89B September 2011 – August 2025
The extended program header attributes section contains three parts:
Figure 19-1 Format of the Extended Program Header Attributes SectionThe first part is a vector of Elf32_TI_PHAttrs, terminated by PHA_NULL. This is followed by the FLBD part and the NTBS part. If used, pha_un.pha_offset shall point into the FLBD or NTBS parts using byte offsets relative to the beginning of the section. FLBD and NTBS can be empty if there are no tags that access the pha_offset field.