SPRU514Z July 2001 – October 2023 SM320F28335-EP
The following example demonstrates how you can control diagnostic messages issued by the compiler. You control the linker diagnostic messages in a similar manner.
int one();
int I;
int main()
{
switch (I){
case 1;
return one ();
break;
default:
return 0;
break;
}
}If you invoke the compiler with the --quiet option, this is the result:
"err.c", line 9: warning: statement is unreachable
"err.c", line 12: warning: statement is unreachableBecause it is standard programming practice to include break statements at the end of each case arm to avoid the fall-through condition, these warnings can be ignored. Using the --display_error_number option, you can find out the diagnostic identifier for these warnings. Here is the result:
[err.c]
"err.c", line 9: warning #111-D: statement is unreachable
"err.c", line 12: warning #111-D: statement is unreachable
Next, you can use the diagnostic identifier of 111 as the argument to the --diag_remark option to treat this warning as a remark. This compilation produces no diagnostic messages (because remarks are disabled by default).
You can suppress any non-fatal errors, but be careful to make sure you only suppress diagnostic messages that you understand and are known not to affect the correctness of your program.