SPRUI03F June 2015 – August 2025
Initialize 32-Bit Integers
.intvalue1[, ... , valuen ]
.uintvalue1[, ... , valuen ]
.long value1[, ... ,valuen ]
.ulong value1[, ... ,valuen ]
.wordvalue1[, ... , valuen ]
.uwordvalue1[, ... , valuen ]
The .int, .unint, .long, .ulong, .word, and .uword directives place one or more values into consecutive words in the current section. Each value is placed in a 32-bit word by itself and is aligned on a word boundary. A value can be either:
A value can be either an absolute or a relocatable expression. If an expression is relocatable, the assembler generates a relocation entry that refers to the appropriate symbol; the linker can then correctly patch (relocate) the reference. This allows you to initialize memory with pointers to variables or labels.
If you use a label with these directives, it points to the first word that is initialized.
When you use these directives in a .struct/.endstruct sequence, they define a member's size; they do not initialize memory. See the .struct/.endstruct/.tag topic.
This example uses the .int directive to initialize words. Notice that the symbol SYMPTR puts the symbol's address in the object code and generates a relocatable reference (indicated by the - character appended to the object word).
1 00000000 .space 73h
2 00000000 .bss PAGE, 128
3 00000080 .bss SYMPTR, 3
4 00000074 003C12E4 INST: LDW.D2 *++B15[0],A0
5 00000078 0000000A .int 10, SYMPTR, -1, 35 + 'a', INST
0000007c 00000080-
00000080 FFFFFFFF
00000084 00000084
00000088 00000074'
This example initializes two 32-bit fields and defines DAT1 to point to the first location. The contents of the resulting 32-bit fields are FFFABCDh and 141h.
1 00000000 FFFFABCD DAT1: .long 0FFFFABCDh,'A'+100h
00000004 00000141
This example initializes five words. The symbol WordX points to the first word.
1 00000000 00000C80 ;WordX .word 3200,1+'AB',-'AF',0F410h,'A'
00000004 00004242
00000008 FFFFB9BF
0000000c 0000F410
00000010 00000041