SPRUIG6L January 2018 – March 2025
When using C7000 Host Emulation to program for C7000, compiler errors and warnings will differ from those seen when compiling the same code with the C7000 compiler. Due to the complex implementation of some of the C7000’s features in Host Emulation, the following sections define some key terms needed to help decipher some Host Emulation compiler errors you may see.
This section also discusses Host Emulation compiler errors and warnings that may be emitted when attempting to use C7000 Host Emulation specific syntax and constructs. Cases that may not trigger compiler errors or warnings are also described.