SPRUIG6L January 2018 – March 2025
The C7000 Host Emulation package consists of C++ source and header files used to drive the features provided by the C7000 compiler.
Depending on the desired host, the source files may need to be built on the host prior to compiling a C7000 program. Detailed instructions on how to build source on different hosts are provided in the sections that follow.
Familiarity with the C7000 C/C++ Optimizing Compiler User's Guide (SPRUIG8) and the C7000 Runtime Support Library is required to fully understand the content in this guide and to use Host Emulation successfully.