SPRUIG8K January 2018 – March 2025
The syntax of assignment statements in the linker is similar to that of assignment statements in the C language:
| symbol | = | expression; | assigns the value of expression to symbol |
| symbol | + = | expression; | adds the value of expression to symbol |
| symbol | - = | expression; | subtracts the value of expression from symbol |
| symbol | * = | expression; | multiplies symbol by expression |
| symbol | / = | expression; | divides symbol by expression |
The symbol should be defined externally. If it is not, the linker defines a new symbol and enters it into the symbol table. The expression must follow the rules defined in Section 12.5.9.3. Assignment statements must terminate with a semicolon.
The linker processes assignment statements after it allocates all the output sections. Therefore, if an expression contains a symbol, the address used for that symbol reflects the symbol's address in the executable output file.
For example, suppose a program reads data from one of two tables identified by two external symbols, Table1 and Table2. The program uses the symbol cur_tab as the address of the current table. The cur_tab symbol must point to either Table1 or Table2. You can use a linker assignment statement to assign cur_tab at link time:
prog.c.obj /* Input file */
cur_tab = Table1; /* Assign cur_tab to one of the tables */