SPRUIG8K January 2018 – March 2025
The compiler translates a source module into an object file. It may place all of the functions into a single code section, or it may create multiple code sections. The benefit of multiple code sections is that the linker may omit unused functions from the executable.
When the linker collects code to be placed into an executable file, it cannot split code sections. If the compiler did not use multiple code sections, and any function in a particular module needs to be linked into the executable, then all functions in that module are linked in, even if they are not used.
Suppose a library *.c.obj file contains a signed divide routine and an unsigned divide routine. If the application requires only signed division, then only the signed divide routine is required for linking. If only one code section is used, both the signed and unsigned routines are linked in since they exist in the same *.c.obj file.
The --gen_func_subsections compiler option remedies this problem by placing each function in a file in its own subsection. Thus, only the functions that are referenced in the application are linked into the final executable. This can result in an overall code size reduction.
However, be aware that using the --gen_func_subsections compiler option can result in overall code size growth if all or nearly all functions are being referenced. This is because any section containing code must be aligned to a 64-byte boundary to support the branching mechanism. When the --gen_func_subsections option is not used, all functions in a source file are usually placed in a common section which is aligned. When --gen_func_subsections is used, each function defined in a source file is placed in a unique section. Each of the unique sections requires alignment. If all the functions in the file are required for linking, code size may increase due to the additional alignment padding for the individual subsections. Thus, the --gen_func_subsections compiler option is advantageous for use with libraries where normally only a limited number of the functions in a file are used in any one executable. The alternative to using the --gen_func_subsections option is to place each function in its own file.
The default is off if this option is not used. If this option is used without specifying "on" or "off", the default is on.