SPRUIV4D May 2020 – May 2024
If the compiler is not using the specialized C7000 instructions you would like it to
use, or if the operation is not easily expressed in C (for example, saturated add),
there may be an intrinsic available for use in C/C++ code. The available intrinsics
appear in the .h files in the include directory of the compiler
installation directory.