SPRUJ53A April 2024 – June 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
Table 20-6 lists the memory-mapped registers for the EQEP_REGS registers. All register offset addresses not listed in Table 20-6 should be considered as reserved locations and the register contents should not be modified.
Offset | Acronym | Register Name | Write Protection | Section |
---|---|---|---|---|
0h | QPOSCNT | Position Counter | Go | |
2h | QPOSINIT | Position Counter Init | Go | |
4h | QPOSMAX | Maximum Position Count | Go | |
6h | QPOSCMP | Position Compare | Go | |
8h | QPOSILAT | Index Position Latch | Go | |
Ah | QPOSSLAT | Strobe Position Latch | Go | |
Ch | QPOSLAT | Position Latch | Go | |
Eh | QUTMR | QEP Unit Timer | Go | |
10h | QUPRD | QEP Unit Period | Go | |
12h | QWDTMR | QEP Watchdog Timer | Go | |
13h | QWDPRD | QEP Watchdog Period | Go | |
14h | QDECCTL | Quadrature Decoder Control | Go | |
15h | QEPCTL | QEP Control | Go | |
16h | QCAPCTL | Qaudrature Capture Control | Go | |
17h | QPOSCTL | Position Compare Control | Go | |
18h | QEINT | QEP Interrupt Control | Go | |
19h | QFLG | QEP Interrupt Flag | Go | |
1Ah | QCLR | QEP Interrupt Clear | Go | |
1Bh | QFRC | QEP Interrupt Force | Go | |
1Ch | QEPSTS | QEP Status | Go | |
1Dh | QCTMR | QEP Capture Timer | Go | |
1Eh | QCPRD | QEP Capture Period | Go | |
1Fh | QCTMRLAT | QEP Capture Latch | Go | |
20h | QCPRDLAT | QEP Capture Period Latch | Go | |
30h | REV | QEP Revision Number | Go | |
32h | QEPSTROBESEL | QEP Strobe select register | Go | |
34h | QMACTRL | QMA Control register | Go | |
36h | QEPSRCSEL | QEP Source Select Register | Go |
Complex bit access types are encoded to fit into small table cells. Table 20-7 shows the codes that are used for access types in this section.
Access Type | Code | Description |
---|---|---|
Read Type | ||
R | R | Read |
R-0 | R -0 | Read Returns 0s |
Write Type | ||
W | W | Write |
W1C | W 1C | Write 1 to clear |
W1S | W 1S | Write 1 to set |
Reset or Default Value | ||
-n | Value after reset or the default value | |
Register Array Variables | ||
i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. |
QPOSCNT is shown in Figure 20-26 and described in Table 20-8.
Return to the Summary Table.
Position Counter
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QPOSCNT | |||||||||||||||||||||||||||||||
R/W-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | QPOSCNT | R/W | 0h | Position Counter This 32-bit position counter register counts up/down on every eQEP pulse based on direction input. This counter acts as a position integrator whose count value is proportional to position from a give reference point. This Register acts as a Read ONLY register while counter is counting up/down. Note: It is recommended to only write to the position counter register (QPOSCNT) during initialization, i.e. when the eQEP position counter is disabled (QPEN bit of QEPCTL is zero). Once the position counter is enabled (QPEN bit is one), writing to the eQEP position counter register (QPOSCNT) may cause unexpected results. Reset type: SYSRSn |
QPOSINIT is shown in Figure 20-27 and described in Table 20-9.
Return to the Summary Table.
Position Counter Init
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QPOSINIT | |||||||||||||||||||||||||||||||
R/W-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | QPOSINIT | R/W | 0h | Position Counter Init This register contains the position value that is used to initialize the position counter based on external strobe or index event. The position counter can be initialized through software. Writes to this register should always be full 32-bit writes. Reset type: SYSRSn |
QPOSMAX is shown in Figure 20-28 and described in Table 20-10.
Return to the Summary Table.
Maximum Position Count
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QPOSMAX | |||||||||||||||||||||||||||||||
R/W-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | QPOSMAX | R/W | 0h | Maximum Position Count This register contains the maximum position counter value. Writes to this register should always be full 32-bit writes. Reset type: SYSRSn |
QPOSCMP is shown in Figure 20-29 and described in Table 20-11.
Return to the Summary Table.
Position Compare
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QPOSCMP | |||||||||||||||||||||||||||||||
R/W-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | QPOSCMP | R/W | 0h | Position Compare The position-compare value in this register is compared with the position counter (QPOSCNT) to generate sync output and/or interrupt on compare match. Writes to this register should always be full 32-bit writes. Reset type: SYSRSn |
QPOSILAT is shown in Figure 20-30 and described in Table 20-12.
Return to the Summary Table.
Index Position Latch
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QPOSILAT | |||||||||||||||||||||||||||||||
R-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | QPOSILAT | R | 0h | Index Position Latch The position-counter value is latched into this register on an index event as defined by the QEPCTL[IEL] bits. Reset type: SYSRSn |
QPOSSLAT is shown in Figure 20-31 and described in Table 20-13.
Return to the Summary Table.
Strobe Position Latch
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QPOSSLAT | |||||||||||||||||||||||||||||||
R-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | QPOSSLAT | R | 0h | Strobe Position Latch The position-counter value is latched into this register on a strobe event as defined by the QEPCTL[SEL] bits. Reset type: SYSRSn |
QPOSLAT is shown in Figure 20-32 and described in Table 20-14.
Return to the Summary Table.
Position Latch
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QPOSLAT | |||||||||||||||||||||||||||||||
R-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | QPOSLAT | R | 0h | Position Latch The position-counter value is latched into this register on a unit time out event. Reset type: SYSRSn |
QUTMR is shown in Figure 20-33 and described in Table 20-15.
Return to the Summary Table.
QEP Unit Timer
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QUTMR | |||||||||||||||||||||||||||||||
R/W-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | QUTMR | R/W | 0h | QEP Unit Timer This register acts as time base for unit time event generation. When this timer value matches the unit time period value a unit time event is generated. Writes to this register should always be full 32-bit writes. Reset type: SYSRSn |
QUPRD is shown in Figure 20-34 and described in Table 20-16.
Return to the Summary Table.
QEP Unit Period
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QUPRD | |||||||||||||||||||||||||||||||
R/W-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | QUPRD | R/W | 0h | QEP Unit Period This register contains the period count for the unit timer to generate periodic unit time events. These events latch the eQEP position information at periodic intervals and optionally generate an interrupt. Writes to this register should always be full 32-bit writes. Reset type: SYSRSn |
QWDTMR is shown in Figure 20-35 and described in Table 20-17.
Return to the Summary Table.
QEP Watchdog Timer
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
QWDTMR | |||||||
R/W-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QWDTMR | |||||||
R/W-0h | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-0 | QWDTMR | R/W | 0h | QEP Watchdog Timer This register acts as time base for the watchdog to detect motor stalls. When this timer value matches with the watchdog's period value a watchdog timeout interrupt is generated. This register is reset upon edge transition in quadrature-clock indicating the motion. Reset type: SYSRSn |
QWDPRD is shown in Figure 20-36 and described in Table 20-18.
Return to the Summary Table.
QEP Watchdog Period
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
QWDPRD | |||||||
R/W-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QWDPRD | |||||||
R/W-0h | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-0 | QWDPRD | R/W | 0h | QEP Watchdog Period This register contains the time-out count for the eQEP peripheral watch dog timer. When the watchdog timer value matches the watchdog period value, a watchdog timeout interrupt is generated. Reset type: SYSRSn |
QDECCTL is shown in Figure 20-37 and described in Table 20-19.
Return to the Summary Table.
Quadrature Decoder Control
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
QSRC | SOEN | SPSEL | XCR | SWAP | IGATE | QAP | |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QBP | QIP | QSP | RESERVED | QIDIRE | |||
R/W-0h | R/W-0h | R/W-0h | R-0h | R/W-0h | |||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-14 | QSRC | R/W | 0h | Position-counter source selection Reset type: SYSRSn 0h (R/W) = Quadrature count mode (QCLK = iCLK, QDIR = iDIR) 1h (R/W) = Direction-count mode (QCLK = xCLK, QDIR = xDIR) 2h (R/W) = UP count mode for frequency measurement (QCLK = xCLK, QDIR = 1) 3h (R/W) = DOWN count mode for frequency measurement (QCLK = xCLK, QDIR = 0) |
13 | SOEN | R/W | 0h | Sync output-enable Reset type: SYSRSn 0h (R/W) = Disable position-compare sync output 1h (R/W) = Enable position-compare sync output |
12 | SPSEL | R/W | 0h | Sync output pin selection Reset type: SYSRSn 0h (R/W) = Index pin is used for sync output 1h (R/W) = Strobe pin is used for sync output |
11 | XCR | R/W | 0h | External Clock Rate Reset type: SYSRSn 0h (R/W) = 2x resolution: Count the rising/falling edge 1h (R/W) = 1x resolution: Count the rising edge only |
10 | SWAP | R/W | 0h | CLK/DIR Signal Source for Position Counter Reset type: SYSRSn 0h (R/W) = Quadrature-clock inputs are not swapped 1h (R/W) = Quadrature-clock inputs are swapped |
9 | IGATE | R/W | 0h | Index pulse gating option Reset type: SYSRSn 0h (R/W) = Disable gating of Index pulse 1h (R/W) = Gate the index pin with strobe |
8 | QAP | R/W | 0h | QEPA input polarity Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Negates QEPA input |
7 | QBP | R/W | 0h | QEPB input polarity Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Negates QEPB input |
6 | QIP | R/W | 0h | QEPI input polarity Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Negates QEPI input |
5 | QSP | R/W | 0h | QEPS input polarity Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Negates QEPS input |
4-1 | RESERVED | R | 0h | Reserved |
0 | QIDIRE | R/W | 0h | 0 - Compatible mode, Behavior same as existing devices 1 - Enhancement for Direction change during Index will be enabled: On QEPI direction change, the incoming posedge of QA can erroneously update/reset the position counter of the eQEP. This bit only needs to be enabled if the application requires a direction change occurring at the same time as an incoming QEPI signal, or when erroneous PC resets are observed. Reset type: SYSRSn |
QEPCTL is shown in Figure 20-38 and described in Table 20-20.
Return to the Summary Table.
QEP Control
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
FREE_SOFT | PCRM | SEI | IEI | ||||
R/W-0h | R/W-0h | R/W-0h | R/W-0h | ||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
SWI | SEL | IEL | QPEN | QCLM | UTE | WDE | |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-14 | FREE_SOFT | R/W | 0h | Emulation mode Reset type: SYSRSn 0h (R/W) = QPOSCNT behavior Position counter stops immediately on emulation suspend 0h (R/W) = QWDTMR behavior Watchdog counter stops immediately 0h (R/W) = QUTMR behavior Unit timer stops immediately 0h (R/W) = QCTMR behavior Capture Timer stops immediately 1h (R/W) = QPOSCNT behavior Position counter continues to count until the rollover 1h (R/W) = QWDTMR behavior Watchdog counter counts until WD period match roll over 1h (R/W) = QUTMR behavior Unit timer counts until period rollover 1h (R/W) = QCTMR behavior Capture Timer counts until next unit period event 2h (R/W) = QPOSCNT behavior Position counter is unaffected by emulation suspend 2h (R/W) = QWDTMR behavior Watchdog counter is unaffected by emulation suspend 2h (R/W) = QUTMR behavior Unit timer is unaffected by emulation suspend 2h (R/W) = QCTMR behavior Capture Timer is unaffected by emulation suspend 3h (R/W) = Same as FREE_SOFT_2 |
13-12 | PCRM | R/W | 0h | Postion counter reset Reset type: SYSRSn 0h (R/W) = Position counter reset on an index event 1h (R/W) = Position counter reset on the maximum position 2h (R/W) = Position counter reset on the first index event 3h (R/W) = Position counter reset on a unit time event |
11-10 | SEI | R/W | 0h | Strobe event initialization of position counter Reset type: SYSRSn 0h (R/W) = Does nothing (action disabled) 1h (R/W) = Does nothing (action disabled) 2h (R/W) = Initializes the position counter on rising edge of the QEPS signal 3h (R/W) = Clockwise Direction: Initializes the position counter on the rising edge of QEPS strobe Counter Clockwise Direction: Initializes the position counter on the falling edge of QEPS strobe |
9-8 | IEI | R/W | 0h | Index event init of position count Reset type: SYSRSn 0h (R/W) = Do nothing (action disabled) 1h (R/W) = Do nothing (action disabled) 2h (R/W) = Initializes the position counter on the rising edge of the QEPI signal (QPOSCNT = QPOSINIT) 3h (R/W) = Initializes the position counter on the falling edge of QEPI signal (QPOSCNT = QPOSINIT) |
7 | SWI | R/W | 0h | Software init position counter Reset type: SYSRSn 0h (R/W) = Do nothing (action disabled) 1h (R/W) = Initialize position counter (QPOSCNT=QPOSINIT). This bit is not cleared automatically |
6 | SEL | R/W | 0h | Strobe event latch of position counter Reset type: SYSRSn 0h (R/W) = The position counter is latched on the rising edge of QEPS strobe (QPOSSLAT = POSCCNT). Latching on the falling edge can be done by inverting the strobe input using the QSP bit in the QDECCTL register 1h (R/W) = Clockwise Direction: Position counter is latched on rising edge of QEPS strobe Counter Clockwise Direction: Position counter is latched on falling edge of QEPS strobe |
5-4 | IEL | R/W | 0h | Index event latch of position counter (software index marker) Reset type: SYSRSn 0h (R/W) = Reserved 1h (R/W) = Latches position counter on rising edge of the index signal 2h (R/W) = Latches position counter on falling edge of the index signal 3h (R/W) = Software index marker. Latches the position counter and quadrature direction flag on index event marker. The position counter is latched to the QPOSILAT register and the direction flag is latched in the QEPSTS[QDLF] bit. This mode is useful for software index marking. |
3 | QPEN | R/W | 0h | Quadrature position counter enable/software reset Reset type: SYSRSn 0h (R/W) = Reset the eQEP peripheral internal operating flags/read-only registers. Control/configuration registers are not disturbed by a software reset. When QPEN is disabled, some flags in the QFLG register do not get reset or cleared and show the actual state of that flag. 1h (R/W) = eQEP position counter is enabled |
2 | QCLM | R/W | 0h | QEP capture latch mode Reset type: SYSRSn 0h (R/W) = Latch on position counter read by CPU. Capture timer and capture period values are latched into QCTMRLAT and QCPRDLAT registers when CPU reads the QPOSCNT register. 1h (R/W) = Latch on unit time out. Position counter, capture timer and capture period values are latched into QPOSLAT, QCTMRLAT and QCPRDLAT registers on unit time out. |
1 | UTE | R/W | 0h | QEP unit timer enable Reset type: SYSRSn 0h (R/W) = Disable eQEP unit timer 1h (R/W) = Enable unit timer |
0 | WDE | R/W | 0h | QEP watchdog enable Reset type: SYSRSn 0h (R/W) = Disable the eQEP watchdog timer 1h (R/W) = Enable the eQEP watchdog timer |
QCAPCTL is shown in Figure 20-39 and described in Table 20-21.
Return to the Summary Table.
Qaudrature Capture Control
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CEN | RESERVED | ||||||
R/W-0h | R-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | CCPS | UPPS | |||||
R-0h | R/W-0h | R/W-0h | |||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15 | CEN | R/W | 0h | Enable eQEP capture Reset type: SYSRSn 0h (R/W) = eQEP capture unit is disabled 1h (R/W) = eQEP capture unit is enabled |
14-7 | RESERVED | R | 0h | Reserved |
6-4 | CCPS | R/W | 0h | eQEP capture timer clock prescaler Reset type: SYSRSn 0h (R/W) = CAPCLK = SYSCLKOUT/1 1h (R/W) = CAPCLK = SYSCLKOUT/2 2h (R/W) = CAPCLK = SYSCLKOUT/4 3h (R/W) = CAPCLK = SYSCLKOUT/8 4h (R/W) = CAPCLK = SYSCLKOUT/16 5h (R/W) = CAPCLK = SYSCLKOUT/32 6h (R/W) = CAPCLK = SYSCLKOUT/64 7h (R/W) = CAPCLK = SYSCLKOUT/128 |
3-0 | UPPS | R/W | 0h | Unit position event prescaler Reset type: SYSRSn 0h (R/W) = UPEVNT = QCLK/1 1h (R/W) = UPEVNT = QCLK/2 2h (R/W) = UPEVNT = QCLK/4 3h (R/W) = UPEVNT = QCLK/8 4h (R/W) = UPEVNT = QCLK/16 5h (R/W) = UPEVNT = QCLK/32 6h (R/W) = UPEVNT = QCLK/64 7h (R/W) = UPEVNT = QCLK/128 8h (R/W) = UPEVNT = QCLK/256 9h (R/W) = UPEVNT = QCLK/512 Ah (R/W) = UPEVNT = QCLK/1024 Bh (R/W) = UPEVNT = QCLK/2048 Ch (R/W) = Reserved Dh (R/W) = Reserved Eh (R/W) = Reserved Fh (R/W) = Reserved |
QPOSCTL is shown in Figure 20-40 and described in Table 20-22.
Return to the Summary Table.
Position Compare Control
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
PCSHDW | PCLOAD | PCPOL | PCE | PCSPW | |||
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | |||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
PCSPW | |||||||
R/W-0h | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15 | PCSHDW | R/W | 0h | Position compare of shadow enable Reset type: SYSRSn 0h (R/W) = Shadow disabled, load Immediate 1h (R/W) = Shadow enabled |
14 | PCLOAD | R/W | 0h | Position compare of shadow load Reset type: SYSRSn 0h (R/W) = Load on QPOSCNT = 0 1h (R/W) = Load when QPOSCNT = QPOSCMP |
13 | PCPOL | R/W | 0h | Polarity of sync output Reset type: SYSRSn 0h (R/W) = Active HIGH pulse output 1h (R/W) = Active LOW pulse output |
12 | PCE | R/W | 0h | Position compare enable/disable Reset type: SYSRSn 0h (R/W) = Disable position compare unit 1h (R/W) = Enable position compare unit |
11-0 | PCSPW | R/W | 0h | Select-position-compare sync output pulse width Reset type: SYSRSn 0h (R/W) = 1 * 4 * SYSCLKOUT cycles 1h (R/W) = 2 * 4 * SYSCLKOUT cycles FFFh (R/W) = 4096 * 4 * SYSCLKOUT cycles |
QEINT is shown in Figure 20-41 and described in Table 20-23.
Return to the Summary Table.
QEP Interrupt Control
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | QMAE | UTO | IEL | SEL | PCM | ||
R-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | ||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
PCR | PCO | PCU | WTO | QDC | QPE | PCE | RESERVED |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-13 | RESERVED | R | 0h | Reserved |
12 | QMAE | R/W | 0h | QMA Error Interrupt enable Reset type: SYSRSn 0h (R/W) = Interrupt is disabled 1h (R/W) = Interrupt is enabled |
11 | UTO | R/W | 0h | Unit time out interrupt enable Reset type: SYSRSn 0h (R/W) = Interrupt is disabled 1h (R/W) = Interrupt is enabled |
10 | IEL | R/W | 0h | Index event latch interrupt enable Reset type: SYSRSn 0h (R/W) = Interrupt is disabled 1h (R/W) = Interrupt is enabled |
9 | SEL | R/W | 0h | Strobe event latch interrupt enable Reset type: SYSRSn 0h (R/W) = Interrupt is disabled 1h (R/W) = Interrupt is enabled |
8 | PCM | R/W | 0h | Position-compare match interrupt enable Reset type: SYSRSn 0h (R/W) = Interrupt is disabled 1h (R/W) = Interrupt is enabled |
7 | PCR | R/W | 0h | Position-compare ready interrupt enable Reset type: SYSRSn 0h (R/W) = Interrupt is disabled 1h (R/W) = Interrupt is enabled |
6 | PCO | R/W | 0h | Position counter overflow interrupt enable Reset type: SYSRSn 0h (R/W) = Interrupt is disabled 1h (R/W) = Interrupt is enabled |
5 | PCU | R/W | 0h | Position counter underflow interrupt enable Reset type: SYSRSn 0h (R/W) = Interrupt is disabled 1h (R/W) = Interrupt is enabled |
4 | WTO | R/W | 0h | Watchdog time out interrupt enable Reset type: SYSRSn 0h (R/W) = Interrupt is disabled 1h (R/W) = Interrupt is enabled |
3 | QDC | R/W | 0h | Quadrature direction change interrupt enable Reset type: SYSRSn 0h (R/W) = Interrupt is disabled 1h (R/W) = Interrupt is enabled |
2 | QPE | R/W | 0h | Quadrature phase error interrupt enable Reset type: SYSRSn 0h (R/W) = Interrupt is disabled 1h (R/W) = Interrupt is enabled |
1 | PCE | R/W | 0h | Position counter error interrupt enable Reset type: SYSRSn 0h (R/W) = Interrupt is disabled 1h (R/W) = Interrupt is enabled |
0 | RESERVED | R | 0h | Reserved |
QFLG is shown in Figure 20-42 and described in Table 20-24.
Return to the Summary Table.
QEP Interrupt Flag
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | QMAE | UTO | IEL | SEL | PCM | ||
R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | ||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
PCR | PCO | PCU | WTO | QDC | PHE | PCE | INT |
R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-13 | RESERVED | R | 0h | Reserved |
12 | QMAE | R | 0h | QMA Error interrupt flag Reset type: SYSRSn 0h (R/W) = No interrupt generated 1h (R/W) = Interrupt was generated |
11 | UTO | R | 0h | Unit time out interrupt flag Reset type: SYSRSn 0h (R/W) = No interrupt generated 1h (R/W) = Set by eQEP unit timer period match |
10 | IEL | R | 0h | Index event latch interrupt flag Reset type: SYSRSn 0h (R/W) = No interrupt generated 1h (R/W) = This bit is set after latching the QPOSCNT to QPOSILAT |
9 | SEL | R | 0h | Strobe event latch interrupt flag Reset type: SYSRSn 0h (R/W) = No interrupt generated 1h (R/W) = This bit is set after latching the QPOSCNT to QPOSSLAT |
8 | PCM | R | 0h | eQEP compare match event interrupt flag Reset type: SYSRSn 0h (R/W) = No interrupt generated 1h (R/W) = This bit is set on position-compare match |
7 | PCR | R | 0h | Position-compare ready interrupt flag Reset type: SYSRSn 0h (R/W) = No interrupt generated 1h (R/W) = This bit is set after transferring the shadow register value to the active position compare register |
6 | PCO | R | 0h | Position counter overflow interrupt flag Reset type: SYSRSn 0h (R/W) = No interrupt generated 1h (R/W) = This bit is set on position counter overflow. |
5 | PCU | R | 0h | Position counter underflow interrupt flag Reset type: SYSRSn 0h (R/W) = No interrupt generated 1h (R/W) = This bit is set on position counter underflow. |
4 | WTO | R | 0h | Watchdog timeout interrupt flag Reset type: SYSRSn 0h (R/W) = No interrupt generated 1h (R/W) = Set by watchdog timeout |
3 | QDC | R | 0h | Quadrature direction change interrupt flag Reset type: SYSRSn 0h (R/W) = No interrupt generated 1h (R/W) = Interrupt was generated |
2 | PHE | R | 0h | Quadrature phase error interrupt flag Reset type: SYSRSn 0h (R/W) = No interrupt generated 1h (R/W) = Set on simultaneous transition of QEPA and QEPB |
1 | PCE | R | 0h | Position counter error interrupt flag Reset type: SYSRSn 0h (R/W) = No interrupt generated 1h (R/W) = Position counter error |
0 | INT | R | 0h | Global interrupt status flag Reset type: SYSRSn 0h (R/W) = No interrupt generated 1h (R/W) = Interrupt was generated |
QCLR is shown in Figure 20-43 and described in Table 20-25.
Return to the Summary Table.
QEP Interrupt Clear
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | QMAE | UTO | IEL | SEL | PCM | ||
R-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | ||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
PCR | PCO | PCU | WTO | QDC | PHE | PCE | INT |
R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-13 | RESERVED | R | 0h | Reserved |
12 | QMAE | R-0/W1S | 0h | Clear QMA Error interrupt flag Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Clears the interrupt flag |
11 | UTO | R-0/W1S | 0h | Clear unit time out interrupt flag Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Clears the interrupt flag |
10 | IEL | R-0/W1S | 0h | Clear index event latch interrupt flag Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Clears the interrupt flag |
9 | SEL | R-0/W1S | 0h | Clear strobe event latch interrupt flag Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Clears the interrupt flag |
8 | PCM | R-0/W1S | 0h | Clear eQEP compare match event interrupt flag Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Clears the interrupt flag |
7 | PCR | R-0/W1S | 0h | Clear position-compare ready interrupt flag Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Clears the interrupt flag |
6 | PCO | R-0/W1S | 0h | Clear position counter overflow interrupt flag Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Clears the interrupt flag |
5 | PCU | R-0/W1S | 0h | Clear position counter underflow interrupt flag Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Clears the interrupt flag |
4 | WTO | R-0/W1S | 0h | Clear watchdog timeout interrupt flag Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Clears the interrupt flag |
3 | QDC | R-0/W1S | 0h | Clear quadrature direction change interrupt flag Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Clears the interrupt flag |
2 | PHE | R-0/W1S | 0h | Clear quadrature phase error interrupt flag Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Clears the interrupt flag |
1 | PCE | R-0/W1S | 0h | Clear position counter error interrupt flag Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Clears the interrupt flag |
0 | INT | R-0/W1S | 0h | Global interrupt clear flag Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Clears the interrupt flag |
QFRC is shown in Figure 20-44 and described in Table 20-26.
Return to the Summary Table.
QEP Interrupt Force
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | QMAE | UTO | IEL | SEL | PCM | ||
R-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | ||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
PCR | PCO | PCU | WTO | QDC | PHE | PCE | RESERVED |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-13 | RESERVED | R | 0h | Reserved |
12 | QMAE | R/W | 0h | Force QMA error interrupt Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Force the interrupt |
11 | UTO | R/W | 0h | Force unit time out interrupt Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Force the interrupt |
10 | IEL | R/W | 0h | Force index event latch interrupt Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Force the interrupt |
9 | SEL | R/W | 0h | Force strobe event latch interrupt Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Force the interrupt |
8 | PCM | R/W | 0h | Force position-compare match interrupt Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Force the interrupt |
7 | PCR | R/W | 0h | Force position-compare ready interrupt Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Force the interrupt |
6 | PCO | R/W | 0h | Force position counter overflow interrupt Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Force the interrupt |
5 | PCU | R/W | 0h | Force position counter underflow interrupt Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Force the interrupt |
4 | WTO | R/W | 0h | Force watchdog time out interrupt Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Force the interrupt |
3 | QDC | R/W | 0h | Force quadrature direction change interrupt Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Force the interrupt |
2 | PHE | R/W | 0h | Force quadrature phase error interrupt Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Force the interrupt |
1 | PCE | R/W | 0h | Force position counter error interrupt Reset type: SYSRSn 0h (R/W) = No effect 1h (R/W) = Force the interrupt |
0 | RESERVED | R | 0h | Reserved |
QEPSTS is shown in Figure 20-45 and described in Table 20-27.
Return to the Summary Table.
QEP Status
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
UPEVNT | FIDF | QDF | QDLF | COEF | CDEF | FIMF | PCEF |
R/W1C-0h | R-0h | R-0h | R-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-8 | RESERVED | R | 0h | Reserved |
7 | UPEVNT | R/W1C | 0h | Unit position event flag Reset type: SYSRSn 0h (R/W) = No unit position event detected 1h (R/W) = Unit position event detected. Write 1 to clear |
6 | FIDF | R | 0h | Direction on the first index marker Status of the direction is latched on the first index event marker. Reset type: SYSRSn 0h (R/W) = Counter-clockwise rotation (or reverse movement) on the first index event 1h (R/W) = Clockwise rotation (or forward movement) on the first index event |
5 | QDF | R | 0h | Quadrature direction flag Reset type: SYSRSn 0h (R/W) = Counter-clockwise rotation (or reverse movement) 1h (R/W) = Clockwise rotation (or forward movement) |
4 | QDLF | R | 0h | eQEP direction latch flag Reset type: SYSRSn 0h (R/W) = Counter-clockwise rotation (or reverse movement) on index event marker 1h (R/W) = Clockwise rotation (or forward movement) on index event marker |
3 | COEF | R/W1C | 0h | Capture overflow error flag Reset type: SYSRSn 0h (R/W) = Overflow has not occurred. 1h (R/W) = Overflow occurred in eQEP Capture timer (QEPCTMR). This bit is cleared by writing a '1'. |
2 | CDEF | R/W1C | 0h | Capture direction error flag Reset type: SYSRSn 0h (R/W) = Capture direction error has not occurred. 1h (R/W) = Direction change occurred between the capture position event. This bit is cleared by writing a '1'. |
1 | FIMF | R/W1C | 0h | First index marker flag Reset type: SYSRSn 0h (R/W) = First index pulse has not occurred. 1h (R/W) = Set by first occurrence of index pulse. This bit is cleared by writing a '1'. |
0 | PCEF | R | 0h | Position counter error flag. This bit is not sticky and it is updated for every index event. Reset type: SYSRSn 0h (R/W) = No error occurred during the last index transition 1h (R/W) = Position counter error |
QCTMR is shown in Figure 20-46 and described in Table 20-28.
Return to the Summary Table.
QEP Capture Timer
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
QCTMR | |||||||
R/W-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QCTMR | |||||||
R/W-0h | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-0 | QCTMR | R/W | 0h | This register provides time base for edge capture unit. Reset type: SYSRSn |
QCPRD is shown in Figure 20-47 and described in Table 20-29.
Return to the Summary Table.
QEP Capture Period
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
QCPRD | |||||||
R/W-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QCPRD | |||||||
R/W-0h | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-0 | QCPRD | R/W | 0h | This register holds the period count value between the last successive eQEP position events Reset type: SYSRSn |
QCTMRLAT is shown in Figure 20-48 and described in Table 20-30.
Return to the Summary Table.
QEP Capture Latch
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
QCTMRLAT | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QCTMRLAT | |||||||
R-0h | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-0 | QCTMRLAT | R | 0h | The eQEP capture timer value can be latched into this register on two events viz., unit timeout event, reading the eQEP position counter. Reset type: SYSRSn |
QCPRDLAT is shown in Figure 20-49 and described in Table 20-31.
Return to the Summary Table.
QEP Capture Period Latch
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
QCPRDLAT | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QCPRDLAT | |||||||
R-0h | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-0 | QCPRDLAT | R | 0h | eQEP capture period value can be latched into this register on two events viz., unit timeout event, reading the eQEP position counter. Reset type: SYSRSn |
REV is shown in Figure 20-50 and described in Table 20-32.
Return to the Summary Table.
QEP Revision Number
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||||||||||
R-0-0h | |||||||||||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | MINOR | MAJOR | |||||||||||||
R-0-0h | R-1h | R-1h | |||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-6 | RESERVED | R-0 | 0h | Reserved |
5-3 | MINOR | R | 1h | This field specifies the Minor Revision number for the eQEP IP. Reset type: N/A |
2-0 | MAJOR | R | 1h | This field specifies the Major Revision number for the eQEP IP. Reset type: N/A |
QEPSTROBESEL is shown in Figure 20-51 and described in Table 20-33.
Return to the Summary Table.
QEP Strobe select register
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | STROBESEL | ||||||
R-0-0h | R/W-0h | ||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-2 | RESERVED | R-0 | 0h | Reserved |
1-0 | STROBESEL | R/W | 0h | Strobe source select: Reset type: SYSRSn 0h (R/W) = QEP Strobe after polarity mux 1h (R/W) = QEP Strobe after polarity mux 2h (R/W) = QEP Strobe after polarity mux ORed with ADCSOCA 3h (R/W) = QEP Strobe after polarity mux ORed with ADCSOCB |
QMACTRL is shown in Figure 20-52 and described in Table 20-34.
Return to the Summary Table.
QMA Control register
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||||||||||
R-0-0h | |||||||||||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | MODE | ||||||||||||||
R-0-0h | R/W-0h | ||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-3 | RESERVED | R-0 | 0h | Reserved |
2-0 | MODE | R/W | 0h | Select Mode for QMA mode: 000 : QMA Module is bypassed. 001 : QMA Mode-1 operation selected 010 : QMA Mode-2 operation selected 011 : QMA Module is bypassed (reserved) 1xx : QMA Module is bypassed (reserved) Reset type: SYSRSn |
QEPSRCSEL is shown in Figure 20-53 and described in Table 20-35.
Return to the Summary Table.
QEP Source Select Register
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||||||||||
R-0-0h | |||||||||||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
QEPSSEL | QEPISEL | QEPBSEL | QEPASEL | ||||||||||||
R/W-0h | R/W-0h | R/W-0h | R/W-0h | ||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R-0 | 0h | Reserved |
15-12 | QEPSSEL | R/W | 0h | QEP Strobe source select: 0x0: From device Pins (Default). Others: Tied to zero. Reset type: SYSRSn |
11-8 | QEPISEL | R/W | 0h | QEP Index source select: 0x0: Device Pin (Default) 0x1: CMPSS1.CTRIPH 0x2: CMPSS2_LITE.CTRIPH 0x3: CMPSS3_LITE.CTRIPH 0x4: CMPSS4_LITE.CTRIPH 0x5: RSVD 0x6: RSVD 0x7: RSVD 0x8: RSVD 0x9: PWMXBAR.1 0xA:PWMXBAR.2 0xB:PWMXBAR.3 0xC:PWMXBAR.4 0xD:PWMXBAR.5 0xE:PWMXBAR.6 0xF:PWMXBAR.7 Note: eQEP needs to be disabled before configuring these bits as it can lead to unexpected behavior if eQEP is running. Reset type: SYSRSn |
7-4 | QEPBSEL | R/W | 0h | QEPB source select: 0x0: Device Pin (Default) 0x1: CMPSS1.CTRIPH 0x2: CMPSS2_LITE.CTRIPH 0x3: CMPSS3_LITE.CTRIPH 0x4: CMPSS4_LITE.CTRIPH 0x5: RSVD 0x6: RSVD 0x7: RSVD 0x8: RSVD 0x9: PWMXBAR.1 0xA:PWMXBAR.2 0xB:PWMXBAR.3 0xC:PWMXBAR.4 0xD:PWMXBAR.5 0xE:PWMXBAR.6 0xF:PWMXBAR.7 Note: eQEP needs to be disabled before configuring these bits as it can lead to unexpected behavior if eQEP is running. Reset type: SYSRSn |
3-0 | QEPASEL | R/W | 0h | QEPA source select: 0x0: Device Pin (Default) 0x1: CMPSS1.CTRIPH 0x2: CMPSS2_LITE.CTRIPH 0x3: CMPSS3_LITE.CTRIPH 0x4: CMPSS4_LITE.CTRIPH 0x5: RSVD 0x6: RSVD 0x7: RSVD 0x8: RSVD 0x9: PWMXBAR.1 0xA:PWMXBAR.2 0xB:PWMXBAR.3 0xC:PWMXBAR.4 0xD:PWMXBAR.5 0xE:PWMXBAR.6 0xF:PWMXBAR.7 Note: eQEP needs to be disabled before configuring these bits as it can lead to unexpected behavior if eQEP is running. Reset type: SYSRSn |