SPRUJ53A April 2024 – June 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
The I2C module clock determines the frequency at which the I2C module operates. A programmable prescaler in the I2C module divides down the SYSCLK to produce the I2C module clock and this I2C module clock is divided further to produce the I2C controller clock on the SCL pin. Figure 25-3 shows the clock generation diagram for I2C module.
To specify the divide-down value, initialize the IPSC field of the prescaler register, I2CPSC. The resulting frequency is:
The prescaler must be initialized only while the I2C module is in the reset state (IRS = 0 in I2CMDR). The prescaled frequency takes effect only when IRS is changed to 1. Changing the IPSC value while IRS = 1 has no effect.
The controller clock appears on the SCL pin when the I2C module is configured to be a controller on the I2C bus. This clock controls the timing of communication between the I2C module and a target. As shown in Figure 25-3, a second clock divider in the I2C module divides down the module clock to produce the controller clock. The clock divider uses the ICCL value of I2CCLKL to divide down the low portion of the module clock signal and uses the ICCH value of I2CCLKH to divide down the high portion of the module clock signal. See Section 25.1.6 for the controller clock frequency equation.