TIDUDS9B December 2017 – November 2022
Figure 3-24 shows the implementation of the trip feature. As the STO goes low, the trip starts to fall. Within 1.52 ms, the input PWM to the gate driver (and hence the output to the gate of the switching device) is terminated.
Figure 3-24 Validation of Trip Zone Functionality Through
STO2Figure 3-25 shows the rejection of a 1-ms STO low pulse by the design.
Figure 3-25 Effect of Rejection: 1-ms Pulse on
Trip