Texas InstrumentsElectronic Commerce
| What's New? | Purchasing | Quality | Electronic Commerce | Training | A/P |

BAR CODE SPECIFICATION

Supplier Receipt Label Specification
Texas Instruments, Incorporated

Revision A-1.9
November 11, 1996

Table of Contents

1. Introduction and Scope

2. General Specifications

2.1 Shipment Integrity

2.2 Label Format

2.3 Required Data

3. Bar Code Specifications

4. Data Identifiers

5. TI Generic Label Format

5.1 Segments

5.2 Building Blocks

5.3 Label Data

6. How Applied

6.1 Breaking up Line Items

6.2 Consolidating Line Items

6.3 How to Apply Labels

7. Submission Requirements

8. Contacting TI

Appendix A. Sample Labels

Appendix B. AIAG Alternate Label

Appendix C. EIA Alternate Label

Appendix D. ANS Bar Code Print Quality

Appendix E. F.A.C.T. DI Standard

Appendix F Glossary






1. Introduction and Scope

To improve the efficiency and accuracy of our material receipt process, Texas Instruments requires each TI supplier to identify all shipments of material with a Supplier Receipt label. This label does not apply to services type companies. This document is a specification of that label.

This document specifies only the supplier receipt label, which needs to be applied to the packing list for each separate shipment. Some suppliers may be required to apply individual labels to each box of a shipment; these specifications are contained elsewhere.

2. General Specifications

This section contains general information about the data which will be required to produce the label.

2.1 Shipment Integrity

The use of a receipt label allows TI to easily process and credit material received for a single PO line item. Thus, all suppliers who ship material to TI must ensure that each purchase order line item is in a separate container, with a separate receipt label. These requirements are explained further in the "How Applied", section 6.

2.2 Label Format

The format specifications presented in section 5 are based on an emerging bar code label specification from the American National Standards Institute (ANSI). In this document, the ANSI-based label is called the TI Generic Label. All information needed to produce this label is contained within this document and referenced documents.

TI suggests that a supplier follow these guidelines to produce TI Generic Supplier Receipt Labels. However, TI recognizes that some suppliers are already producing labels which meet the Automotive Industry Action Group (AIAG) and Electronic Industries Association (EIA) standards. Thus, TI will accept labels meeting the current AIAG standards from those suppliers who are already producing AIAG labels. Likewise, TI will accept labels meeting current EIA specifications from those suppliers already producing EIA labels. However, both labels must contain the required data set out in this document, and shall be laid out according to the sample labels in Appendix B for the AIAG standard and Appendix C for the EIA standard.

2.3 Required Data

Each Supplier Receipt label, regardless of the format used, contains the following information. How the data is presented (including the Data Identifiers (DI) and start / stop characters) is specified as part of the label format. All fields shall be bar coded unless otherwise noted.





2.3.1 PO and Item Number

TI's Purchase Order number and Item Number from that PO, separated by a plus sign ("+"). Note that the "+" sign is not a normal part of the PO Number, and is used to be consistent with the F.A.C.T. standard. This is a required field.

The Purchase Order Number can be a maximum of 9 characters, the Item Number a maximum of 4. Thus, the maximum length for this field, including the "+" sign, is 14 characters.

2.3.2 Packing List Number

A data block containing the supplier's Packing List number. This field has a maximum of 12 characters. This is a required field.

2.3.3 Part Number

TI's part number for the product being supplied. This field can contain no more than 15 characters, not including the DI, start or stop characters. This is sufficient for nearly all of TI's suppliers. If a supplier will be printing a part number longer than 15 characters, they should contact Texas Instruments for further instruction. This is not a required field.

2.3.4 Customer Part Mark (Finished Goods Only)

This field is required only for Materials and Controls Group suppliers of Finished Goods material having a "mark" code. These suppliers must use the TI Generic label format to include a mark code. This is not a required field.

2.3.5 Quantity

The total quantity of parts contained, measured in the units listed on the purchase order. For Receipt Labels which are supplied on a per-shipment basis, the Quantity is the total quantity in the shipment. If the receipt labels are applied to each individual box, then the Quantity reflects the quantity in the labeled box. This field has a maximum of 9 characters. This is a required field.

2.3.6 Date Shipped

The date the material was shipped, in human readable form only (i.e., no bar code). The date should be of the form "Date Shipped: 21-Jul-96". This is a requested field.

2.3.7 Serial Number

The format, requirements, and identifiers for the Serial Number will be defined by the standards of the using group at Texas Instruments receiving the material. Not a required field.

  1. Manufacturer's Identification Number

The MFG ID# is your company's cage code. If you are a distributor, the MFG ID# is the cage code of the manufacturer of the part you are supplying. This is a required field.

2.3.9 EDl Transaction Number

A label may include a transaction number for use in an Advanced Shipment Notification (ASN) between EDI trading partners. The format and identifier for this number must be mutually agreed upon between the individual suppliers and the group at TI receiving the label. When included, any data on the Supplier Receipt label must be consistent with the data contained in the EDI transmission. This is not a currently required field.

3. Bar Code Specifications

All bar codes appearing on the label, whether printed for TI's use or others, shall meet the specifications contained herein.

The allowable range of the X dimension, (narrow element width) for any bar code on the label shall be 0.010 to 0.017 inch.

The allowable range of the achieved Wide to Narrow Ratio shall be 2.4:1 to 3.2:1.

There shall be a minimum "quiet zone" of 0.25 inch on both sides of each bar code.

The above bar code specifications allow bar code densities between 4 and 7 characters per inch (CPI).

All bar codes shall be Code 3 of 9 (Code 39), and shall be at least a grade "C/10/660" (grade "B/10/660" preferred) overall profile wide, as defined in section 5.3.1.5 of the American National Standard X3.182-1990 Bar Code Print Quality Guideline (see Appendix D for ordering information). The following specifications are needed for this width calculation:

Measurement aperture: 0.010 inch

Inspection wavelength: 660 +/- 10 nanometers

4. Data Identifiers

All bar codes appearing on the label, whether printed for TI's use or others, shall be prefixed by a standard FACT Data Identifier (DI). These Data Identifiers are defined in the current issue of the F.A.C.T. Data Identifier Standard (see Appendix E for ordering information).

The data identifiers for fields defined in this document are:

Field NameData Identifier
PO & Item Number 14K
MFG ID # 17V
Quantity Q
Packing List Number 11K

5. TI Generic Label Format

This section contains the format for the TI Generic Supplier Receipt Label. It describes how to organize the above data on the TI Generic Label.

5.1 Segments

Each label may contain up to four segments. A segment is a collection of related data. Segments are arranged vertically on a label, and are separated by a double ruled horizontal line. The available segments for the label are:

5.1.1 Address Segment

This optional segment contains information a supplier may use for the "From" and "To" addresses for their carrier. TI does not require an address segment on this label, but a supplier may wish to use this segment to provide information for a carrier.

If included, all fields of an address must conform to the standards set out in this document and must be submitted on a sample label to TI for prior approval.

5.1.2 Transaction Segment

This segment contains data originating from the transaction between TI and the supplier, such as the Purchase Order Number and Item Number.

5.1.3 Customer Segment

This segment contains data originating from the customer (TI), such as the TI Part Number.

5.1.4 Supplier Segment

This segment contains information originating from the supplier, such as the quantity of material shipped and lot number.

5.2 Building Blocks

Each segment is divided into Building Blocks. There are two types of building blocks: Regular and Human Readable Only (HRO). Regular building blocks contain a single piece of information, which appears in both human readable and bar code form. HRO building blocks contain only human readable data, and may contain several lines of information. Building blocks are arranged vertically within a segment, and are separated by a single horizontal line.







5.2.1 Regular Building Blocks

As discussed above, regular building blocks contain a single piece of information, (the "field"). The components of a regular building block are:

5.2.1.1 Title

The title for each building block should be printed in small type at the top of the block. A Data Identifier enclosed in parentheses (see section 4) shall immediately follow the title. The title should be in a typeface which is at least 0.06 inch and no more than 0.13 inch in height.

5-2.1.2 Human Readable

A human readable version of the field value, without the data identifier prefix, shall appear below the title. It should be indented approximately 0.75 inch from the left side of the label. The typeface must be at least 0.20 inch in height.

5.2.1.3 Bar code

Some building blocks are Human Readable only, and do not contain bar codes. All others shall contain a single bar code of the field value, prefixed by the building block data identifier. The bar code must be at least 0.50 inch in height, and meet the specifications in section 3.

5.2.2 Human Readable Only Building Blocks

HRO building blocks supply data in human readable fashion only, and do not contain bar codes. There may be one or more lines of data within the building block, and each line within a given building block should be in the same typeface.

5.3 Label Data

The following data may appear on the TI Generic Supplier Receipt Label :

5.3..l Address segment

TI does not require any information in the address segment, see 5.1.1.

5.3.2 Transaction Segment

The transaction segment contains the following data:

1. PO and Item Number. The title for this building block is:

"Purchase Order and Item (14K)".

2. Packing List Number. The title shall be:

"Packing List Number (11K)".

3. EDI Transaction Number, if supplied.

5.3.3 Customer Segment

The customer segment contains the following data:

1. Part Number (if supplied). The title for this field is:

"Customer Part No (P)".

2. Customer Part Mark (if supplied). The title for this building block is:

"Customer (21P)".

5.3.4 Supplier Segment

The supplier segment contains the following building blocks:

1. Quantity. The title for this field is:

"Quantity (Q)".

2. Date Shipped. An HRO building block (not bar coded), containing the date the material was shipped. The date should be of the form:

"Date Shipped: 21-Jul-95".

3. Manufacturer's Identification Number, (cage code). The title for this field is:

"MFG ID # (17V)".

4. Serial Number, if supplied.

5.3.5 Label Size

The label width shall be from 4 inches to 5 inches wide, with 4.5 inches being the preferred width. The supplier is responsible for selecting a label width which can accommodate the bar codes for all building blocks listed herein (especially the 15 character TI part number, if required, and the 14 character PO & Item number), including Data Identifiers, start/stop characters and quiet zones.

The label height shall be from 4 to 8 inches, depending upon the needs of the supplier.

Each block shall be 1.0 inch +/- 0.2 inch; the actual height shall be determined the supplier. However, the building block height should be the same for building blocks within the same segment.










6. How Applied

This section describes how to apply the Supplier Receipt label. Each group at TI may also have specific requirements regarding how the label is applied. If a supplier receives instructions from its buyer, either in the cover letter attached to this document or otherwise, the supplier should follow those instructions. In particular, a group may specify which of the two methods described in section 6.1 should be used.

When all material for a single line item is shipped in a single container, a single Supplier Receipt label should be applied to the packing slip, reflecting the total quantity of the shipment. When material for a line item is divided or consolidated, a supplier should consult the following sections:

6.1 Breaking Up Line Item

When a line item is divided into multiple containers (in loose cartons, for example), the supplier may label the material according to one of the following two methods:

1. One Supplier Receipt Label Per Carton. Each carton has a Supplier Receipt label which reflects the quantity of parts in the labeled container. The sum of the quantities for all containers for a given PO Line Item should equal the quantity on the packing slip.

2. One Label per Shipment, with Carton Counts. Each carton has the following Human Readable Information:

1) PO Number and Item Number

2) Quantity

3) An indication of the carton number in the shipment. This indication should be of the form "1 of 5", showing the carton number and the total number of boxes in the shipment.

In this case, a single supplier receipt label must be applied to the whole shipment, reflecting the total quantity in the shipment, attached to the back of the pack slip.

6.2 Consolidating Line Items

A supplier may consolidate multiple line items into a larger container. In this case, each line item must be packed in a separate inner container with a separate Supplier Receipt Label for each item attached to the back of the packing slip. When shipped together, each individual line item label may have the same Packing List Number.








6.3 How to Apply Labels

This section describes the physical application of the Supplier Receipt label, after its location has been determined by the preceding section.

6.3.1 Packing List

The label may be applied to the front or back of the packing list for the shipment, provided it does not cover any data on the packing list. However, the bar code shall not be folded or creased when it is received by TI.

6.3.2 Container In Shipment

The Supplier Receipt label may also be applied to any container of the shipment, provided it is clearly visible and that there are no other bar code labels applied to the container.

6.3.3 Applying Labels to Containers

When applied to a standard box, labels should be affixed wrinkle-free to the upper right hand comer of a narrow side of the box, so it will be visible when stored on a shelf. For boxes with a square footprint, the label may be applied to any side. The top edge of the Label should be between 0.75 inch and 2 inches from the top edge of the carton. The right edge of the label should be between 0.75 inch and 2 inches from the right edge of the carton.

When the container is not a box, it should be affixed or attached in such a way as to be clearly visible and undamaged when received. For reels, coils and other unit loads which lack a smooth surface, the Label should be affixed to a string or wire tag, which is in turn attached to the container.

7. Submission Requirements

All suppliers are required to submit sample labels to Texas Instruments for approval. Each supplier shall submit ten original (not photocopied) labels for approval by Texas Instruments. These sample labels should be sent to the address indicated on the cover letter attached to this document. Each label should have different information in the fields.

8. Contacting TI

Any supplier who requires more information about complying with these specifications should contact their buyer or the contacts shown on the cover letter..








Appendix A

TI Generic Label



Appendix B

AIAG Alternate Label



Appendix C

EIA Alternate Label



Appendix D

American National Standard X3.182.1990

Bar Code Print Quality Guideline





_____________________________________________________________________________________

Order Form

To: Customer Fill out your address in the blanks below, and enclose a check for $47.00 ($42.00+$5.00 Shipping and Handling) made out to ANSI. Then, mail it together with this order form to the following address:

ANSI

Attn: Sales Department

11 West 42nd Street

New York, NY 10036

You may call the Sales Department at ANSI by dialing (212) 642-4900 for more information.

To: ANSI Please send a copy of the publication ANS X3.182.1990 to the address listed below:

Address: Company:

Name:

Address:

City/State/Zip












Appendix E

F.A.C.T. Data Identifier Standard





_____________________________________________________________________________________

Order Form

To: Customer Fill out your address in the blanks below, and enclose a check for $56.00 ($50.00+$6.00 Shipping and Handling) made out to ANSI. Then, mail it together with this order form to the following address:

ANSI

Attn: Sales Department

11 West 42nd Street

New York, NY 10036

You may call the Sales Department at ANSI by dialing (212) 642-4900 for more information.

To: ANSI Please send a copy of the publication FACT 1 to the address listed below:

Address: Company:

Name:

Address:

City/State/Zip












Appendix F

Glossary of Terms

AIAG Automotive Industry Action Group

Building Block In the TI-Generic Label, an area of the label containing at most one bar coded field. Building blocks are arranged vertically and separated by a single-ruled line.

Character A letter, digit or other special symbol.

AIM Automatic Identification Manufacturer's, Inc.

ANSI The American National Standards Institute, a non governmental organization responsible for the administration of voluntary national standards.

Data Field See Field

Data Identifier A string of Characters

EDI Electronic Data Interchange. A means whereby trading partners communicate transaction information electronically via a standard format.

EIA Electronic Industries Association

F.A.C.T. Federation of Automated Coding Technologies.

Field In this document, an entity of data on a bar code label. The title, human readable and bar code information for a single piece of data are considered a single field.

Item Number The individual line item number from a P.O. used to order a single part number.

Label Format In this document, the standard used to determine how the data is printed on the label. The three label formats discussed are TI Generic, EIA and AIAG.

Mark Code A supplemental number used by TI, together with the part number, to identify finished goods parts.

Narrow Element

Width The average width of a narrow element in a bar code symbol.

Packing List Number A number used on the packing list document by a supplier to identify a single shipment of material.

The P.O. Number A number used by TI to identify the Purchase Order used to order material. A PO may contain multiple items.

Print Quality The measure of compliance of a bar code symbol to the requirements of dimensional tolerance, edge roughness, spots, voids, reflectance, quiet zone and data encoded.

Quiet Zone One of two spaces which precede the start character and follow the stop character in a bar code symbol No printing of any kind is allowed in the quiet zone.

Serial Number A unique number used to identify a carton, unit load or shipment. Serial numbers are usually generated by the supplier of the material.

Segment A collection of related data on the TI Generic label Segments contain one or more building blocks, and are separated by a double ruled horizontal line.

Start/Stop Character A special bar code character or characters which provide a scanner with start and stop reading instructions as well as a way of determining the scanning direction.

TI Generic label The label format described in this document, based on emerging standards from ANSI.

Transport Package A package intended for the transportation of one or more articles,. or smaller packages, or bulk Material

Unit Load A number of filled transport packages or other items that are held together by means such as a pallet, slip sheet, strapping, interlocking, glue, shrink wrap, stretch wrap or net wrap to make them suitable for transportation and storage as a unit. The term is also used to describe a single large item suitable packaged for transportation and storage.

USS Code 39 The Universal Symbology Specification for Code 39.

Wide:Narrow Ratio The ratio of the average width of a wide element in a bar code ratio to the Narrow Element Width.

X Dimension The Narrow Element Width of a bar code.



TI HomeSearchFeedbackecomm home


© Copyright 1996 Texas Instruments Incorporated. All rights reserved.
Trademarks