The Instant Microcontroller Lab
“Everything you need to start teaching with MSP430 Low Power Microcontrollers”

 

Texas Instruments MSP430 devices are the easiest and most effective platforms for teaching microcontrollers. The MSP430 is a modern RISC device with a powerful instruction set and lean efficient architecture. It is ultra-low power and very easy to program. After using the MSP430 you will never want to use an “8051” or an 8 bit device ever again!

 

In Europe, TI will be donating 150 of these Instant Microcontroller Labs between now and the closing date of 16th December 2009.  

The Instant Microcontroller lab includes:    

 

1 x MSP430 Teaching ROM  (Lit. Code: SSQC017)

http://ti.com/europe/university 

 

1 x Code Composer Essentials Professional  (MSP-CCE430PRO)

http://focus.ti.com/docs/toolsw/folders/print/msp-cce430pro.html 

 

1 x MSP430FG4618 Experimenter Board (MSP-EXP430FG4618)

http://focus.ti.com/docs/toolsw/folders/print/msp-exp430fg4618.html 

 

1 x MSP430 USB Debugging Interface (MSP-FET430UIF)

http://focus.ti.com/docs/toolsw/folders/print/msp-fet430uif.html 

 

1 x MSP430 RF2500 Development Tool (EZ430-RF2500)

http://focus.ti.com/docs/toolsw/folders/print/ez430-rf2500.html

 

4 x MSP430 USB Development Tool (EZ430-F2012)

http://focus.ti.com/docs/toolsw/folders/print/ez430-f2013.html

 

Our MSP430 “Teaching ROM” provides all the materials you need to begin straight away: Lecture Slides, Course Notes, Tutorials, Tests and fully debugged Code Examples. These materials have already been tried and tested in a Student Lab environment.

 

Bring your students into the 21st century with a microcontroller that is uniquely suited to today’s environmentally conscious world!   

 

To apply for an Instant Microcontoller Lab go to our online registration form here and provide us with a detailed description of your planned use of the lab as well as your shipping details.

 

For more information on the European University Program, visit our site here

Thanks and Best Regards,


    The European University Program Team

 

 
To ensure delivery to your inbox, please add tiprime@dlep14.itg.ti.com to your address book or safe sender list.

The platform bar is a trademark of Texas Instruments.
All other trademarks are the property of their respective owners.