Design Support

 614 views

The bq76200 is a low-power, high-side, N-Channel MOSFET driver that can be utilized in a variety of FET configurations to assist the user’s battery protection system from faults such as a cell’s undervoltage and overvoltage or a short circuit. The following material is aimed to portray various applications of the bq76200 with several different configurations of FETs, pack voltages, and cell counts that will represent the driver’s functionality under each setup. These configurations were chosen to portray the optimal functionality of the part as well as to define the parameters of applicability in order to present examples where a setup may need debugging.