Design Support

 53 views

This document discusses the power consumption of the Texas Instruments TMS320DM640, TMS320DM641, TMS320DM642, and TMS320DM643 digital signal processors (DSPs). Power consumption on these devices is highly application- dependent, so a spreadsheet is provided to model power consumption for a user's application. To get good results from the spreadsheet, realistic usage parameters must be entered. The low-core voltage and other power design optimizations allow these DSPs to operate with industry-leading performance, while maintaining a low power-to-performance ratio.< P > The data presented in this document is actual measured power consumption for the DM642 silicon revision 1.0. < P >This application report contains a spreadsheet that can be downloaded from this link: http://www-s.ti.com/sc/psheets/spra962f/spra962f.zip. The spreadsheet should be used to correct power numbers given in the following table for the DM640, DM641, and DM643. For example, the DM640 and DM641 only have a 32-bit EMIF decreasing the overall power consumption.

Associated Files: