Design Support

 

The purpose of this design note is to show how the FEC decoding implemented in HW on the CC1100, CC1100E, CC1101, CC1110Fx, CC1111Fx, CC1150, CC2500, CC2510Fx, CC2511Fx, and CC2550 can be implemented in SW. This is in particular very important for the CC430Fx device, which has the same radio as the CC1101 and CC1110/11Fx but without HW FEC included.