Other Parts Discussed in Thread: XTR106 , XTR116 Hi,
Looking for a mV(bridge output) to 4-20mA loop transmitter IC options that is suitable for new designs.
XTR106/115/116/117 etc showing last minute to buy. Do you have any new active options available…
Part Number: ADS125H02
Hi
Please let us know the terminal connection for the 4~20mA and 0~10v dc for sensor measurements
Thank you in advance.
Regards
Thiagu
HI Purushottam,
As Clemens has mentioned, on a 2-wire current transmitter, the IRET or local GND of the 2-wire current transmitter, needs to float with respect to the loop ground. The IRET (local ground) potential moves as a function of the current loop…
Part Number: DAC8750 Other Parts Discussed in Thread: TIPD101 , TIPD102 , DAC8771 Hello Expert,
I have some question for configuration about below.
Could you please check and send it guide and document?
The DAC8750 is currently being used as the Source…
HI Iien,
The total current consumption of the XTR current transmitter circuitry, that is, the current consumption of the XTR116 plus the consumption of the bridge sensor, and all the associated circuits driving the XTR116, must be less than 4mA.
The…
Part Number: MSPM0L1306 Other Parts Discussed in Thread: SYSCONFIG Hello,
I am hoping to configure the MSPM0 device as a Controller for 2 peripherals.
This would be a 4 wire connection between controller and peripheral with separate CS lines as shown below…
Hi,
After designing the circuit with reference to 4-20mA discrete components, further simulating the circuit with Voltage regulator LM317 as per required 12V output from voltage regulator. I am maintaining the ratio as suggested by Clemens, and it is…
Other Parts Discussed in Thread: DRV5053 Good morning Technical
I have a hydraulic motor mounted on a horizontal plate with an output shaft that has a bevel gear. The other end of the shaft protrudes from the non-drive end of the hydraulic motor enough…
Part Number: ADS1120 Hi,
in your Application Note " A Basic Guide to RTD Measurements" in section 2.7.1, a circuit is shown for 2 RTDs needing a 5 channel ADC. As AIN2 and AIN3 are shorted together at the RTD inputs, would it be possible to modify…
2-wire transmitters are loop powered devices most commonly used to monitor a remote process with no access to a local supply. Two analog signal wires carry both the analog output signal, and power for the sensor/monitoring circuitry and transmitter. The…