The files contained in this archive are:

1.) 3574_78.s43 - assembly language file for IAR Embedded Workbench
2.) msp430x14x.h - header file containing register definitions for the MSP430F149 device
3.) TLC357X.h - header file containing definitions for functions / registers of the ADC
4.) Legal.asm - Texas Instruments Legal Disclaimer - Please Read!
4.) readme.txt - this file

Please create a dedicated project folder under your X:\IAR\EW23\430\FET_Examples directory.
Extract the files in this archive to the project folder.  Open the IAR Embedded Workbench 
environment and create a new project.  Use the "project - add files" menu to locate your
project directory and be sure to include the .s43 file.  The necessary include files will
attach themselves to the project.

Under the "Project - Options" menu from the IAR Workbench main screen, set the following options:

1.)  Under the "XLINK" menu,  click on the "Include" tab and check the "Override default" option.
Use the browse button to locate the "msp430F149A.xcl" file which should be in the 
X:\IAR\ew23\430\icc430\ directory.  (Note: replace "X" with the drive letter where the software tool 
is installed)

2.)  Under the "C-SPY" menu,  Choose the "Flash Emulation Tool" from the driver drop down box.  
Check the "Use description file" box and browse to the directory that contains the msp430F149.ddf
file.  It should be located in the "X:\IAR\ew23\430\cw430" directory. 

Please feel free to email "dataconvapps@list.ti.com" if you have questions or need assistance.