TMS320x281x BOOT ROM Source

This download includes the source of the boot ROM contents
on TMS320x281x devices. 

=============================================================
IMPORTANT NOTES: 

Since the boot ROM source as frozen, the header file format 
has changed.  That is the header files used by the boot ROM do not
match those used in C281x C/C++ Header Files and Peripheral Examples 
(SPRC097)

The source code references a "K1" device.  This was an internal
test chip.  The source code for the K1 has been conditionally 
compiled out.  It only remains since the source code was frozen
at the time of release.
=============================================================

The .zip contains all source including the project file, 
header files and the .out file used to generate the boot
ROM contents. 

By default, the boot ROM source will be placed in the
C:\tidcs\c28\boot_rom\281x directory.