TMS320x280x BOOT ROM Source

This download includes the source of the boot ROM contents
on TMS320x280x devices. 

For each version of the boot ROM there is one .zip file
included where the version of the release is reflected
in the name of the .zip file.  The boot ROM version
on a particular device is stored in memory location
0x3FFFBA in the boot ROM.

The .zip contains all source including the project file, 
header files and the .out file used to generate the boot
ROM contents. 

By default, the boot ROM source will be placed in the
C:\tidcs\c28\boot_rom\280x directory.