#include <stdbool.h>#include <stdint.h>#include <inc/hw_types.h>#include <inc/hw_memmap.h>#include <inc/hw_aon_batmon.h>#include <driverlib/debug.h>Go to the source code of this file.
Macros | |
| #define | AON_BATMON_CYCLE_32 AON_BATMON_MEASCFG_PER_32CYC |
| #define | AON_BATMON_CYCLE_16 AON_BATMON_MEASCFG_PER_16CYC |
| #define | AON_BATMON_CYCLE_8 AON_BATMON_MEASCFG_PER_8CYC |
| #define | AON_BATMON_CYCLE_CONT AON_BATMON_MEASCFG_PER_CONT |
Functions | |
| __STATIC_INLINE void | AONBatMonEnable (void) |
| Enable the temperatur and battery monitoring. More... | |
| __STATIC_INLINE void | AONBatMonDisable (void) |
| Disable the temperatur and battery monitoring. More... | |
| __STATIC_INLINE void | AONBatMonMeasurementCycleSet (uint32_t ui32Cycle) |
| Adjust the measurement cycle for the temperature and the battery voltage. More... | |
| __STATIC_INLINE uint32_t | AONBatMonMeasurementCycleGet (void) |
| Get the measurement cycle for the temperature and the battery voltage. More... | |
| __STATIC_INLINE void | AONBatMonBatteryTrimSet (uint32_t ui32TrimP0, uint32_t ui32TrimP1) |
| Set the trim values for the battery voltage calculation. More... | |
| __STATIC_INLINE void | AONBatMonTemperatureTrimSet (uint32_t ui32TrimP0, uint32_t ui32TrimP1, uint32_t ui32TrimP2) |
| Set the trim values for the temperature calculation. More... | |
| __STATIC_INLINE uint32_t | AONBatMonTemperatureGet (void) |
| Get the current temperature measurement. More... | |
| int32_t | AON_BatmonTempGetDegC (void) |
| Get the current temperature measurement as a signed value in Deg Celsius. More... | |
| __STATIC_INLINE uint32_t | AONBatMonBatteryVoltageGet (void) |
| Get the battery monitor measurement. More... | |
| __STATIC_INLINE bool | AONBatMonNewBatteryMeasureReady (void) |
| Check if battery monitor measurement has changed. More... | |
| __STATIC_INLINE bool | AONBatMonNewTempMeasureReady (void) |
| Check if temperature monitor measurement has changed. More... | |