#include <driverlib/aux_adc.h>#include <inc/hw_memmap.h>#include <inc/hw_aux_wuc.h>#include <driverlib/adi.h>#include <driverlib/event.h>Go to the source code of this file.
Functions | |
| void | AUXADCDisable (void) |
| Disables the ADC. More... | |
| void | AUXADCEnableAsync (uint32_t refSource, uint32_t trigger) |
| Enables the ADC for asynchronous operation. More... | |
| void | AUXADCEnableSync (uint32_t refSource, uint32_t sampleTime, uint32_t trigger) |
| Enables the ADC for synchronous operation. More... | |
| void | AUXADCFlushFifo (void) |
| Flushes the ADC FIFO. More... | |
| uint32_t | AUXADCReadFifo (void) |
| Waits for and returns the first sample in the ADC FIFO. More... | |