Functions | |
| ProtocolBitVector_t | ChipInfo_GetSupportedProtocol_BV (void) |
| Returns bit vector showing supported protocols. More... | |
| __STATIC_INLINE bool | ChipInfo_SupportsBLE (void) |
| Returns true if the chip supports the BLE protocol. More... | |
| __STATIC_INLINE bool | ChipInfo_SupportsIEEE_802_15_4 (void) |
| Returns true if the chip supports the IEEE 802.15.4 protocol. More... | |
| __STATIC_INLINE bool | ChipInfo_SupportsPROPRIETARY (void) |
| Returns true if the chip supports propriatary protocols. More... | |
| PackageType_t | ChipInfo_GetPackageType (void) |
| Returns package type. More... | |
| __STATIC_INLINE bool | ChipInfo_PackageTypeIs4x4 (void) |
| Returns true if this is a 4x4mm chip. More... | |
| __STATIC_INLINE bool | ChipInfo_PackageTypeIs5x5 (void) |
| Returns true if this is a 5x5mm chip. More... | |
| __STATIC_INLINE bool | ChipInfo_PackageTypeIs7x7 (void) |
| Returns true if this is a 7x7mm chip. More... | |
| __STATIC_INLINE uint32_t | ChipInfo_GetDeviceIdHwRevCode (void) |
| Returns the internal chip HW revision code. More... | |
| ChipFamily_t | ChipInfo_GetChipFamily (void) |
| Returns chip family member. More... | |
| __STATIC_INLINE bool | ChipInfo_ChipFamilyIsCC26xx (void) |
| Returns true if this chip is member of the CC26xx family. More... | |
| __STATIC_INLINE bool | ChipInfo_ChipFamilyIsCC13xx (void) |
| Returns true if this chip is member of the CC13xx family. More... | |
| HwRevision_t | ChipInfo_GetHwRevision (void) |
| Returns chip HW revision. More... | |
| __STATIC_INLINE bool | ChipInfo_HwRevisionIs_1_0 (void) |
| Returns true if HW revision for this chip is 1.0. More... | |
| __STATIC_INLINE bool | ChipInfo_HwRevisionIs_GTEQ_2_0 (void) |
| Returns true if HW revision for this chip is 2.0 or greater. More... | |
| __STATIC_INLINE bool | ChipInfo_HwRevisionIs_2_0 (void) |
| Returns true if HW revision for this chip is 2.0. More... | |
| __STATIC_INLINE bool | ChipInfo_HwRevisionIs_2_1 (void) |
| Returns true if HW revision for this chip is 2.1. More... | |
| __STATIC_INLINE bool | ChipInfo_HwRevisionIs_2_2 (void) |
| Returns true if HW revision for this chip is 2.2. More... | |
| __STATIC_INLINE bool | ChipInfo_HwRevisionIs_GTEQ_2_2 (void) |
| Returns true if HW revision for this chip is 2.2 or greater. More... | |
| void | ThisCodeIsBuiltForCC26xxHwRev22AndLater_HaltIfViolated (void) |
| Verifies that current chip is built for CC26xx HwRev 2.2 or later and never returns if violated. More... | |
Enumerations | |
| enum | ProtocolBitVector_t { PROTOCOL_Unknown = 0, PROTOCOLBIT_BLE = 0x02, PROTOCOLBIT_IEEE_802_15_4 = 0x04, PROTOCOLBIT_Proprietary = 0x08 } |
| Enumeration identifying the protocols supported. More... | |
| enum | PackageType_t { PACKAGE_Unknown = -1, PACKAGE_4x4 = 0, PACKAGE_5x5 = 1, PACKAGE_7x7 = 2 } |
| Package type enumeration. More... | |
| enum | ChipFamily_t { FAMILY_Unknown = -1, FAMILY_CC26xx = 0, FAMILY_CC13xx = 1 } |
| Chip family enumeration. More... | |
| enum | HwRevision_t { HWREV_Unknown = -1, HWREV_1_0 = 0, HWREV_2_0 = 1, HWREV_2_1 = 2, HWREV_2_2 = 3 } |
| HW revision enumeration. More... | |
| __STATIC_INLINE bool ChipInfo_ChipFamilyIsCC13xx | ( | void | ) |
Returns true if this chip is member of the CC13xx family.
true if this chip is member of the CC13xx family, false otherwise. Definition at line 260 of file chipinfo.h.
| __STATIC_INLINE bool ChipInfo_ChipFamilyIsCC26xx | ( | void | ) |
Returns true if this chip is member of the CC26xx family.
true if this chip is member of the CC26xx family, false otherwise. Definition at line 246 of file chipinfo.h.
Referenced by ThisCodeIsBuiltForCC26xxHwRev22AndLater_HaltIfViolated().
| ChipFamily_t ChipInfo_GetChipFamily | ( | void | ) |
Returns chip family member.
Definition at line 90 of file chipinfo.c.
Referenced by ChipInfo_ChipFamilyIsCC13xx(), and ChipInfo_ChipFamilyIsCC26xx().
| __STATIC_INLINE uint32_t ChipInfo_GetDeviceIdHwRevCode | ( | void | ) |
Returns the internal chip HW revision code.
Definition at line 209 of file chipinfo.h.
Referenced by ChipInfo_GetChipFamily(), and ChipInfo_GetHwRevision().
| HwRevision_t ChipInfo_GetHwRevision | ( | void | ) |
Returns chip HW revision.
Definition at line 111 of file chipinfo.c.
Referenced by ChipInfo_HwRevisionIs_1_0(), ChipInfo_HwRevisionIs_2_0(), ChipInfo_HwRevisionIs_2_1(), ChipInfo_HwRevisionIs_2_2(), ChipInfo_HwRevisionIs_GTEQ_2_0(), and ChipInfo_HwRevisionIs_GTEQ_2_2().
| PackageType_t ChipInfo_GetPackageType | ( | void | ) |
Returns package type.
Definition at line 67 of file chipinfo.c.
Referenced by ChipInfo_PackageTypeIs4x4(), ChipInfo_PackageTypeIs5x5(), and ChipInfo_PackageTypeIs7x7().
| ProtocolBitVector_t ChipInfo_GetSupportedProtocol_BV | ( | void | ) |
Returns bit vector showing supported protocols.
Definition at line 56 of file chipinfo.c.
Referenced by ChipInfo_SupportsBLE(), ChipInfo_SupportsIEEE_802_15_4(), and ChipInfo_SupportsPROPRIETARY().
| __STATIC_INLINE bool ChipInfo_HwRevisionIs_1_0 | ( | void | ) |
Returns true if HW revision for this chip is 1.0.
true if HW revision for this chip is 1.0, false otherwise. Definition at line 297 of file chipinfo.h.
| __STATIC_INLINE bool ChipInfo_HwRevisionIs_2_0 | ( | void | ) |
Returns true if HW revision for this chip is 2.0.
true if HW revision for this chip is 2.0, false otherwise. Definition at line 325 of file chipinfo.h.
| __STATIC_INLINE bool ChipInfo_HwRevisionIs_2_1 | ( | void | ) |
Returns true if HW revision for this chip is 2.1.
true if HW revision for this chip is 2.1, false otherwise. Definition at line 339 of file chipinfo.h.
| __STATIC_INLINE bool ChipInfo_HwRevisionIs_2_2 | ( | void | ) |
Returns true if HW revision for this chip is 2.2.
true if HW revision for this chip is 2.2, false otherwise. Definition at line 353 of file chipinfo.h.
| __STATIC_INLINE bool ChipInfo_HwRevisionIs_GTEQ_2_0 | ( | void | ) |
Returns true if HW revision for this chip is 2.0 or greater.
true if HW revision for this chip is 2.0 or greater, false otherwise. Definition at line 311 of file chipinfo.h.
| __STATIC_INLINE bool ChipInfo_HwRevisionIs_GTEQ_2_2 | ( | void | ) |
Returns true if HW revision for this chip is 2.2 or greater.
true if HW revision for this chip is 2.2 or greater, false otherwise. Definition at line 367 of file chipinfo.h.
Referenced by ThisCodeIsBuiltForCC26xxHwRev22AndLater_HaltIfViolated().
| __STATIC_INLINE bool ChipInfo_PackageTypeIs4x4 | ( | void | ) |
Returns true if this is a 4x4mm chip.
true if this is a 4x4mm chip, false otherwise. Definition at line 167 of file chipinfo.h.
| __STATIC_INLINE bool ChipInfo_PackageTypeIs5x5 | ( | void | ) |
Returns true if this is a 5x5mm chip.
true if this is a 5x5mm chip, false otherwise. Definition at line 181 of file chipinfo.h.
| __STATIC_INLINE bool ChipInfo_PackageTypeIs7x7 | ( | void | ) |
Returns true if this is a 7x7mm chip.
true if this is a 7x7mm chip, false otherwise. Definition at line 195 of file chipinfo.h.
| __STATIC_INLINE bool ChipInfo_SupportsBLE | ( | void | ) |
Returns true if the chip supports the BLE protocol.
true if supporting the BLE protocol, false otherwise. Definition at line 102 of file chipinfo.h.
| __STATIC_INLINE bool ChipInfo_SupportsIEEE_802_15_4 | ( | void | ) |
Returns true if the chip supports the IEEE 802.15.4 protocol.
true if supporting the IEEE 802.15.4 protocol, false otherwise. Definition at line 116 of file chipinfo.h.
| __STATIC_INLINE bool ChipInfo_SupportsPROPRIETARY | ( | void | ) |
Returns true if the chip supports propriatary protocols.
true if supporting propriatary protocols, false otherwise. Definition at line 130 of file chipinfo.h.
| void ThisCodeIsBuiltForCC26xxHwRev22AndLater_HaltIfViolated | ( | void | ) |
Verifies that current chip is built for CC26xx HwRev 2.2 or later and never returns if violated.
Definition at line 161 of file chipinfo.c.
Referenced by trimDevice().
| enum ChipFamily_t |
Chip family enumeration.
| Enumerator | |
|---|---|
| FAMILY_Unknown |
Chip family member is unknown. |
| FAMILY_CC26xx |
This chip is a CC26xx family member. |
| FAMILY_CC13xx |
This chip is a CC13xx family member. |
Definition at line 221 of file chipinfo.h.
| enum HwRevision_t |
HW revision enumeration.
Definition at line 270 of file chipinfo.h.
| enum PackageType_t |
Package type enumeration.
| Enumerator | |
|---|---|
| PACKAGE_Unknown |
Current chip type is unknown. |
| PACKAGE_4x4 |
This is a 4x4mm chip. |
| PACKAGE_5x5 |
This is a 5x5mm chip. |
| PACKAGE_7x7 |
This is a 7x7mm chip. |
Definition at line 141 of file chipinfo.h.
| enum ProtocolBitVector_t |
Enumeration identifying the protocols supported.
Definition at line 75 of file chipinfo.h.