Functions | |
| __STATIC_INLINE uint32_t | ADIStatusGet (uint32_t ui32Base) |
| Get the status of an ADI module. More... | |
| __STATIC_INLINE void | ADIConfigSet (uint32_t ui32Base, uint32_t ui32Config, bool bProtect) |
| Configure the ADI Slave. More... | |
| __STATIC_INLINE void | ADISync (uint32_t ui32Base) |
| Synchronize the ADI slave. More... | |
| __STATIC_INLINE void | ADIProtect (uint32_t ui32Base) |
| Protect an ADI slave configuration by locking the configuration register access. More... | |
| __STATIC_INLINE void | ADI8RegWrite (uint32_t ui32Base, uint32_t ui32Reg, uint8_t ui8Val) |
| Write an 8 bit value to a register in an ADI slave. More... | |
| __STATIC_INLINE void | ADI16RegWrite (uint32_t ui32Base, uint32_t ui32Reg, uint16_t ui16Val) |
| Write a 16 bit value to 2 registers in the ADI slave. More... | |
| __STATIC_INLINE void | ADI32RegWrite (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val) |
| Write a 32 bit value to 4 registers in the ADI slave. More... | |
| __STATIC_INLINE uint32_t | ADI8RegRead (uint32_t ui32Base, uint32_t ui32Reg) |
| Read the value of an 8 bit register in the ADI slave. More... | |
| __STATIC_INLINE uint32_t | ADI16RegRead (uint32_t ui32Base, uint32_t ui32Reg) |
| Read the value in a 16 bit register. More... | |
| __STATIC_INLINE uint32_t | ADI32RegRead (uint32_t ui32Base, uint32_t ui32Reg) |
| Read the value in a 32 bit register. More... | |
| __STATIC_INLINE void | ADI8BitsSet (uint32_t ui32Base, uint32_t ui32Reg, uint8_t ui8Val) |
| Set specific bits in a single 8 bit ADI register. More... | |
| __STATIC_INLINE void | ADI16BitsSet (uint32_t ui32Base, uint32_t ui32Reg, uint16_t ui16Val) |
| Set specific bits in 2 x 8 bit ADI slave registers. More... | |
| __STATIC_INLINE void | ADI32BitsSet (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val) |
| Set specific bits in 4 x 8 bit ADI slave registers. More... | |
| __STATIC_INLINE void | ADI8BitsClear (uint32_t ui32Base, uint32_t ui32Reg, uint8_t ui8Val) |
| Clear specific bits in an 8 bit ADI register. More... | |
| __STATIC_INLINE void | ADI16BitsClear (uint32_t ui32Base, uint32_t ui32Reg, uint16_t ui16Val) |
| Clear specific bits in two 8 bit ADI register. More... | |
| __STATIC_INLINE void | ADI32BitsClear (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val) |
| Clear specific bits in four 8 bit ADI register. More... | |
| __STATIC_INLINE void | ADI4SetValBit (uint32_t ui32Base, uint32_t ui32Reg, bool bWriteHigh, uint8_t ui8Mask, uint8_t ui8Val) |
| Set a value on any 4 bits inside an 8 bit register in the ADI slave. More... | |
| __STATIC_INLINE void | ADI8SetValBit (uint32_t ui32Base, uint32_t ui32Reg, uint16_t ui16Mask, uint16_t ui16Val) |
| Set a value on any bits inside an 8 bit register in the ADI slave. More... | |
| __STATIC_INLINE void | ADI16SetValBit (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Mask, uint32_t ui32Val) |
| Set a value on any bits inside an 2 x 8 bit register aligned on a half-word (byte) boundary in the ADI slave. More... | |
| __STATIC_INLINE void ADI16BitsClear | ( | uint32_t | ui32Base, |
| uint32_t | ui32Reg, | ||
| uint16_t | ui16Val | ||
| ) |
Clear specific bits in two 8 bit ADI register.
This function will clear bits in 2 registers in the analog domain. The access to the registers in the analog domain is either 8, 16 or 32 bit aligned, but arranged in chunck of 32 bits. You can only do 16 bit access on registers 0-1 / 2-3, etc. Similarly 32 bit accesses are always performed on register 0-3 / 4-7 etc. Addresses for the registers and values being written to the registers will be truncated according to this access sceme.
| ui32Base | is ADI base address. |
| ui32Reg | is the base registers to clear the bits in. |
| ui16Val | is the 16 bit one-hot encoded value specifying which bits to clear in the registers. |
| __STATIC_INLINE void ADI16BitsSet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Reg, | ||
| uint16_t | ui16Val | ||
| ) |
Set specific bits in 2 x 8 bit ADI slave registers.
This function will set bits in 2 registers in the analog domain. The access to the registers in the analog domain is either 8, 16 or 32 bit aligned, but arranged in chunck of 32 bits. You can only do 16 bit access on registers 0-1 / 2-3, etc. Similarly 32 bit accesses are always performed on register 0-3 / 4-7 etc. Addresses for the registers and values being written to the registers will be truncated according to this access sceme.
| ui32Base | is ADI base address. |
| ui32Reg | is the base register to assert the bits in. |
| ui16Val | is the 16 bit one-hot encoded value specifying which bits to set in the registers. |
| __STATIC_INLINE uint32_t ADI16RegRead | ( | uint32_t | ui32Base, |
| uint32_t | ui32Reg | ||
| ) |
Read the value in a 16 bit register.
This function will read 2 x 8 bit registers in the analog domain and return the value as the lower 16 bits of an uint32_t. The access to the registers in the analog domain is either 8, 16 or 32 bit aligned. You can only do 16 bit access on registers 0-1 / 2-3, etc. Similarly 32 bit accesses are always performed on register 0-3 / 4-7, etc. Addresses for the registers and values being written to the registers will be truncated according to this access sceme.
| ui32Base | is ADI base address. |
| ui32Reg | is the 16 bit register to read. |
uint32_t.| __STATIC_INLINE void ADI16RegWrite | ( | uint32_t | ui32Base, |
| uint32_t | ui32Reg, | ||
| uint16_t | ui16Val | ||
| ) |
Write a 16 bit value to 2 registers in the ADI slave.
This function will write a value to 2 consecutive registers in the analog domain. The access to the registers in the analog domain is either 8, 16 or 32 bit aligned. You can only do 16 bit access on registers 0-1 / 2-3, etc. Similarly 32 bit accesses are always performed on register 0-3 / 4-7, etc. Addresses for the registers and values being written to the registers will be truncated according to this access sceme.
| ui32Base | is ADI base address. |
| ui32Reg | is the register to write. |
| ui16Val | is the 16 bit value to write to the register. |
| __STATIC_INLINE void ADI16SetValBit | ( | uint32_t | ui32Base, |
| uint32_t | ui32Reg, | ||
| uint32_t | ui32Mask, | ||
| uint32_t | ui32Val | ||
| ) |
Set a value on any bits inside an 2 x 8 bit register aligned on a half-word (byte) boundary in the ADI slave.
This function allows 2 byte (16 bit) access to the ADI slave registers.
Use this function to write any value in the range 0-15 bits aligned on a half-word (byte) boundary. Fx. for writing the value 0b101 to bits 1 and 3 the ui32Val = 0x000A and the ui32Mask = 0x000E. Bits 0 and 5-15 will not be affected by the operation, as the corresponding bits are not set in the ui32Mask.
| ui32Base | is the base address of the ADI port. |
| ui32Reg | is the Least Significant Register in the ADI slave that will be affected by the write operation. |
| ui32Mask | is the mask defining which of the 16 bit that should be overwritten. The mask must be defined in the lower half of the 32 bits. |
| ui32Val | is the value to write. The value must be defined in the lower half of the 32 bits. |
| __STATIC_INLINE void ADI32BitsClear | ( | uint32_t | ui32Base, |
| uint32_t | ui32Reg, | ||
| uint32_t | ui32Val | ||
| ) |
Clear specific bits in four 8 bit ADI register.
This function will clear bits in 4 registers in the analog domain. The access to the registers in the analog domain is either 8, 16 or 32 bit aligned, but arranged in chunck of 32 bits. You can only do 16 bit access on registers 0-1 / 2-3, etc. Similarly 32 bit accesses are always performed on register 0-3 / 4-7 etc. Addresses for the registers and values being written to the registers will be truncated according to this access sceme.
| ui32Base | is ADI base address. |
| ui32Reg | is the base registers to clear the bits in. |
| ui32Val | is the 32 bit one-hot encoded value specifying which bits to clear in the registers. |
| __STATIC_INLINE void ADI32BitsSet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Reg, | ||
| uint32_t | ui32Val | ||
| ) |
Set specific bits in 4 x 8 bit ADI slave registers.
This function will set bits in 4 registers in the analog domain. The access to the registers in the analog domain is either 8, 16 or 32 bit aligned, but arranged in chunck of 32 bits. You can only do 16 bit access on registers 0-1 / 2-3, etc. Similarly 32 bit accesses are always performed on register 0-3 / 4-7 etc. Addresses for the registers and values being written to the registers will be truncated according to this access sceme.
| ui32Base | is ADI base address. |
| ui32Reg | is the base register to assert the bits in. |
| ui32Val | is the 32 bit one-hot encoded value specifying which bits to set in the registers. |
| __STATIC_INLINE uint32_t ADI32RegRead | ( | uint32_t | ui32Base, |
| uint32_t | ui32Reg | ||
| ) |
Read the value in a 32 bit register.
This function will read 4 x 8 bit registers in the analog domain and return the value as an uint32_t. The access to the registers in the analog domain is either 8, 16 or 32 bit aligned. You can only do 16 bit access on registers 0-1 / 2-3, etc. Similarly 32 bit accesses are always performed on register 0-3 / 4-7, etc. Addresses for the registers and values being written to the registers will be truncated according to this access sceme.
| ui32Base | is ADI base address. |
| ui32Reg | is the 32 bit register to read. |
| __STATIC_INLINE void ADI32RegWrite | ( | uint32_t | ui32Base, |
| uint32_t | ui32Reg, | ||
| uint32_t | ui32Val | ||
| ) |
Write a 32 bit value to 4 registers in the ADI slave.
This function will write a value to 4 consecutive registers in the analog domain. The access to the registers in the analog domain is either 8, 16 or 32 bit aligned. You can only do 16 bit access on registers 0-1 / 2-3, etc. Similarly 32 bit accesses are always performed on register 0-3 / 4-7, etc. Addresses for the registers and values being written to the registers will be truncated according to this access sceme.
| ui32Base | is ADI base address. |
| ui32Reg | is the register to write. |
| ui32Val | is the 32 bit value to write to the register. |
| __STATIC_INLINE void ADI4SetValBit | ( | uint32_t | ui32Base, |
| uint32_t | ui32Reg, | ||
| bool | bWriteHigh, | ||
| uint8_t | ui8Mask, | ||
| uint8_t | ui8Val | ||
| ) |
Set a value on any 4 bits inside an 8 bit register in the ADI slave.
This function allows halfbyte (4 bit) access to the ADI slave registers. The parameter bWriteHigh determines whether to write to the lower or higher part of the 8 bit register.
Use this function to write any value in the range 0-3 bits aligned on a half byte boundary. Fx. for writing the value 0b101 to bits 1 to 3 the ui8Val = 0xA and the ui8Mask = 0xE. Bit 0 will not be affected by the operation, as the corresponding bit is not set in the ui8Mask.
| ui32Base | is the base address of the ADI port. |
| ui32Reg | is the Least Significant Register in the ADI slave that will be affected by the write operation. |
| bWriteHigh | defines which part of the register to write in.
|
| ui8Mask | is the mask defining which of the 4 bits that should be overwritten. The mask must be defined in the lower half of the 8 bits of the parameter. |
| ui8Val | is the value to write. The value must be defined in the lower half of the 8 bits of the parameter. |
| __STATIC_INLINE void ADI8BitsClear | ( | uint32_t | ui32Base, |
| uint32_t | ui32Reg, | ||
| uint8_t | ui8Val | ||
| ) |
Clear specific bits in an 8 bit ADI register.
This function will clear bits in a register in the analog domain. The access to the registers in the analog domain is either 8, 16 or 32 bit aligned, but arranged in chunck of 32 bits. You can only do 16 bit access on registers 0-1 / 2-3, etc. Similarly 32 bit accesses are always performed on register 0-3 / 4-7 etc. Addresses for the registers and values being written to the registers will be truncated according to this access sceme.
| ui32Base | is ADI base address. |
| ui32Reg | is the base registers to clear the bits in. |
| ui8Val | is the 8 bit one-hot encoded value specifying which bits to clear in the register. |
Definition at line 774 of file adi.h.
Referenced by AUXADCDisable().
| __STATIC_INLINE void ADI8BitsSet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Reg, | ||
| uint8_t | ui8Val | ||
| ) |
Set specific bits in a single 8 bit ADI register.
This function will set bits in a single register in the analog domain. The access to the registers in the analog domain is either 8, 16 or 32 bit aligned, but arranged in chunck of 32 bits. You can only do 16 bit access on registers 0-1 / 2-3, etc. Similarly 32 bit accesses are always performed on register 0-3 / 4-7 etc. Addresses for the registers and values being written to the registers will be truncated according to this access sceme.
| ui32Base | is ADI base address. |
| ui32Reg | is the base register to assert the bits in. |
| ui8Val | is the 8 bit one-hot encoded value specifying which bits to set in the register. |
Definition at line 603 of file adi.h.
Referenced by AUXADCEnableAsync(), and AUXADCEnableSync().
| __STATIC_INLINE uint32_t ADI8RegRead | ( | uint32_t | ui32Base, |
| uint32_t | ui32Reg | ||
| ) |
Read the value of an 8 bit register in the ADI slave.
This function will read an 8 bit register in the analog domain and return the value as the lower 8 bits of an uint32_t. The access to the registers in the analog domain is either 8, 16 or 32 bit aligned. You can only do 16 bit access on registers 0-1 / 2-3, etc. Similarly 32 bit accesses are always performed on register 0-3 / 4-7, etc. Addresses for the registers and values being written to the registers will be truncated according to this access sceme.
| ui32Base | is ADI base address. |
| ui32Reg | is the 8 bit register to read. |
uint32_t.| __STATIC_INLINE void ADI8RegWrite | ( | uint32_t | ui32Base, |
| uint32_t | ui32Reg, | ||
| uint8_t | ui8Val | ||
| ) |
Write an 8 bit value to a register in an ADI slave.
This function will write a value to a single register in the analog domain. The access to the registers in the analog domain is either 8, 16, or 32 bit aligned. You can only do 16 bit access on registers 0-1 / 2-3, etc. Similarly 32 bit accesses are always performed on register 0-3 / 4-7, etc. Addresses for the registers and values being written to the registers will be truncated according to this access sceme.
| ui32Base | is ADI base address. |
| ui32Reg | is the register to write. |
| ui8Val | is the 8 bit value to write to the register. |
| __STATIC_INLINE void ADI8SetValBit | ( | uint32_t | ui32Base, |
| uint32_t | ui32Reg, | ||
| uint16_t | ui16Mask, | ||
| uint16_t | ui16Val | ||
| ) |
Set a value on any bits inside an 8 bit register in the ADI slave.
This function allows byte (8 bit) access to the ADI slave registers.
Use this function to write any value in the range 0-7 bits aligned on a byte boundary. Fx. for writing the value 0b101 to bits 1 and 3 the ui16Val = 0x0A and the ui16Mask = 0x0E. Bits 0 and 5-7 will not be affected by the operation, as the corresponding bits are not set in the ui16Mask.
| ui32Base | is the base address of the ADI port. |
| ui32Reg | is the Least Significant Register in the ADI slave that will be affected by the write operation. |
| ui16Mask | is the mask defining which of the 8 bit that should be overwritten. The mask must be defined in the lower half of the 16 bits. |
| ui16Val | is the value to write. The value must be defined in the lower half of the 16 bits. |
| __STATIC_INLINE void ADIConfigSet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Config, | ||
| bool | bProtect | ||
| ) |
Configure the ADI Slave.
Use this function to configure the interface between the ADI master and the ADI slave. The configuration value for the ADI slave sets the speed of the ADI interface and define if the master should wait for acknowledge from the slave.
If the bProtect parameter is set, the configuration register in the ADI slave is locked for future writes.
bProtect parameter is set, it is no longer possible to modify the configuration register.| ui32Base | is ADI base address. |
| ui32Config | is the configuration of the ADI slave. Value must be a bitwise OR'ed combination of one of each of the two following items:
|
| bProtect | determines if the register access should be protected.
|
| __STATIC_INLINE void ADIProtect | ( | uint32_t | ui32Base | ) |
Protect an ADI slave configuration by locking the configuration register access.
This function will lock the configuration interface to the ADI slave.
| ui32Base | is ADI base address. |
| __STATIC_INLINE uint32_t ADIStatusGet | ( | uint32_t | ui32Base | ) |
Get the status of an ADI module.
This function will return the value of the status register ADI_O_SLAVESTAT which contains status of Request and Acklowledge signals.
| ui32Base | is ADI base address. Allowed values are:
|
| __STATIC_INLINE void ADISync | ( | uint32_t | ui32Base | ) |
Synchronize the ADI slave.
This function will perform a sync on the ADI slave by issuing a NOP ADI command to the master with REQ=0. In other words, the master performs a dummy write request to ensure the master and slave are synchronized.
| ui32Base | is ADI base address. |
| #define ADI_NO_WAIT 0x00000000 |
Definition at line 82 of file adi.h.
Referenced by ADIConfigSet().
| #define ADI_PROTECT 0x00000080 |
Definition at line 95 of file adi.h.
Referenced by ADIConfigSet(), and ADIProtect().
| #define ADI_SLAVE_REGS 16 |
Definition at line 75 of file adi.h.
Referenced by ADI16BitsClear(), ADI16BitsSet(), ADI16RegRead(), ADI16RegWrite(), ADI16SetValBit(), ADI32BitsClear(), ADI32BitsSet(), ADI32RegRead(), ADI32RegWrite(), ADI4SetValBit(), ADI8BitsClear(), ADI8BitsSet(), ADI8RegRead(), ADI8RegWrite(), and ADI8SetValBit().
| #define ADI_SPEED_16 0x00000003 |
Definition at line 87 of file adi.h.
Referenced by ADIConfigSet().
| #define ADI_SPEED_2 0x00000000 |
Definition at line 84 of file adi.h.
Referenced by ADIConfigSet().
| #define ADI_SPEED_4 0x00000001 |
Definition at line 85 of file adi.h.
Referenced by ADIConfigSet().
| #define ADI_SPEED_8 0x00000002 |
Definition at line 86 of file adi.h.
Referenced by ADIConfigSet().
| #define ADI_WAIT_FOR_ACK 0x00000004 |
Definition at line 83 of file adi.h.
Referenced by ADIConfigSet().